Other Parts Discussed in Thread: MSP430G2553
Hai,
We are using DRV870-Q1EVM to drive a 12v DC motor with an external Micro via SPI.
Would like to know if it is possible to interface an external micro to DRV870-Q1EVM through the 14 pin interface provided at the top board? Will the micro MSP430G2553 which is on board interfere the SPI comm from external micro?
And what is the range of PWM period supported by device when it is operating at MODE-3 (Standard PWM Control Interface)?