Recently bought 2 DRV8308EVM developer kits. Had the kits working with the Telcon motor (that came along with the kit) and with an Anaheim motor (another BLDC 3 phase motor). One of the boards has recently thrown a "fault" for no apparent reason (fault LED is on with line pulled low). Resets through the code composer SW does not reset, and there is no indication of why fault is thrown. Is there a way to reset fault or test as to what occurred to throw the fault?