Other Parts Discussed in Thread: DRV8848
Hello,
I am designing a circuit to drive a small latching solenoid at very high speeds. The duty cycle will be 50%, on for 2s, off for 2s. I am looking to cycle the solenoid on-off at a rate of 100Hz or greater.
The solenoid is a Geeplus SIL-0211 : 24Ohms, 4V, 2.7W, 107mA release current. Is the DRV8837 a suitable driver for this application? Are there others I should consider? Can you recommend ways to maximize speed?
Thank you!
Alex