Hi everybody.
I made custom a circuit with DRV8412 and dspic33 family Microcontroller. I use this board with 4 motors DC brushless connected with M1=M2=M3 =0; I use 16KHz pwm.
Motors works at 12V and the signel motor can absorb max 2A.
This is what happend:
The motors are connected to a big machine of 400Kg and they have to lift it. i can reduce the weight from 100kg to 400kg.
When i lift 100kg there is no problem. driver works fine. in this case motors absorb about 700mA.
When i increase the weight to 150kg or more the OTW led indication blink quickly and after a while block the motors. ( just one driver, so 2 motors, the other 2 works fine).
I can reach max 3.3A with 4 motors( so less than 1A to motors), before it the OTW led start to blink.
Attached you can find my electrical scheme. It's just one drive. the other one is exactly the same.