Other Parts Discussed in Thread: DRV8320, DRV8323
I check the datasheet for DRV 8312 and max current is 13.2A. In this case, I can only drive the Motor from 1000 rpm to 2000 rpm. I want to run the Motor at 10000rpm. So I Need a bigger BLDC Driver. Is there anyone can introduce me?