Hi team,
According to the diagram of the DRV10970, My customer want to know below information:
1. The MOSFET is connect to the VM, what's the cap value between the Drain and Source electrode?
2. Is there any requirement for the raising edge for the supply voltage in VM pin. if the raising time is less than 100ns for the 12V supply voltage, will this cause the impulse current in the VM pin. If so, what's the maximum level of impulse current? if there is a equation for this?
Please help to look at above two questions.
Lacey
Thanks a lot!