Dears
1.why there is demand of maximum voltage VM in EQ10 when VM is different from external H-Bridge supply?
2.Where is Equation 10 derive from ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Rick
Here is my understanding,
1、Described in 7.3.10,When VM<12V,VCP =2*VM -1.5; VCP provides High gate driver,so VG=VCP=2*VM-1.5, if HS MOS switched-off,VS = ? if HS MOS switched on,VS=Vbat, so VGS=VG-VS =2*VM-1.5-Vbat<VGS CALMP ,assume VGS CLAMP =10.5V, VGS=2*VM-1.5-Vbat<10.5 ; So VM<(12+Vbat)/2 ; it seems a little difference between with EQ 10.
2、Described in 7.3.10 ,If VM>12V,VCP=VM+9.5V. if HS MOS switched-off,VS = ? if HS MOS switched on,VS=Vbat, so VGS=VG-VS =VM+9.5-Vbat<VGS CALMP ,assume VGS CLAMP =10.5V ,VGS = VM+9.5V-Vbat<10.5V, So VM < 1+BAT ,it seems if VM>12V ,it must be trigger VGS CLAMP.
3、By the way,Described in 7.3.12,VGS trigger VGS CLAMP, The clamping diode will conducting to clamp voltage within 10.5-13V, only if the clamp diode was burn out,then maybe damage FETs
If above viewpoint is right ?and please help answer my question, thanks
Hi Rick
Blow is my understanding:
1、Described in 7.3.10, When VM<12V, VCP=2*VM - 1.5V ,Vcp provides HS Gate driver, VG=VCP=2*vm-1.5V, if HS MOS switch-off, VS=0 ? if HS MOS switched-on,VS=Vbat ,so VGS=VG-VS=2*VM-1.5-Vbat < VGS CLAMP, Assume VGS CLAMP=10.5V, So VGS=2*VM-1.5V-Vbat<10.5V , VM<(12+Vbat)/2, it seems a little differet from EQ10;
2、Described in 7.3.10,When VM>12V,VCP=VM+9.5 =VG,if HS MOS switch-off, VS=0 ? if HS MOS switched-on,VS=Vbat, VGS=VM+9.5-Vbat<VGS CLAMP ,so VM>12V, it is easy to trigger VGS CLAMP;
3、Described in 7.3.12, When VGS trigger VGS CLAMP, the Clamp Diode will conducting to clamp voltage to 10.5-13V, only if Clamp Diode was burn out, it maybe damage FETs.
if above viewpoint ids right ? and please answer my questioin,thanks