• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Applications » Motor Drivers » All Tags » drv8301
Share
Motor Drivers
  • Forum
  • Announcements
  • E2E Wiki

Browse by Tags

Motor Drivers

Welcome to the Motor Drivers Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
drv8301
  • arduino pwm motor driver
  • BLDC motor control
  • Brushless motor control
  • controlCARD
  • DC brush motor
  • drv8302
  • drv8312
  • drv8313
  • DRV8412
  • fault
  • motor
  • Motor Control Development Kit
  • motor driver
  • motor drivers
  • MSP430 Launch pad
  • status register
Related Posts
  • Forum Post: DRV8301 faulting immediately on start-up

    Joe Hlebasko Joe Hlebasko
    I am experimenting with the DVR8301-HC2 kit. I was able to work my through the basic GUI and then the Build steps with the code getting my motor to spin at the right steps. I started to add some code to the existing BLDC_Int project to read the potentiometer to set the speed. I started getting a driver...
    on Dec 3, 2011
  • Wiki Page: Hardware files and software libraries for DRV83x and DRV84x Kits - Where to Find?

    Ryan Kehr Ryan Kehr
    Q: Where do you get the hardware files (schematic, BOM, gerbers, etc.) and software libraries for the DRV83x and DRV84x evaluation kits? A: ControlSUITE http://focus.ti.com/docs/toolsw/folders/print/controlsuite.html Download and install at the link above. After install, you can navigate...
    on Dec 6, 2011
  • Forum Post: Fault and Warning Reporting and Handling in DRV8302

    Joseph Lee90700 Joseph Lee90700
    Dear All, I am debugging using customer board( TMS320F28035 + DRV8302 : DC bus voltage: Max 32V, Phase Current: Max 20A, RPM: Max 3000RPM, PWM= 15kHz, Servo Motor). Unfortunately we found "FAULT" signal as soon as we operated. (The signal pattern of "FAULT" pin is "...
    on Jan 16, 2012
  • Forum Post: DRV8302 and NTSOA

    Mark Berry Mark Berry
    Hello Forum Experts, I wondered if there is any further information available to define the Negative Transient Safe Operating Area for the DRV830x parts. There is a single line comment in the data sheet that says "High side gate drive will survive negative output from bridge up to -10V for...
    on Jan 18, 2012
  • Forum Post: DRV8301/2 dead time setting in 3-input mode.

    Shane Colton Shane Colton
    Does the deadtime setting configured with a resistor on the DTC pin of the DRV8301/8302 also apply in 3-input mode? There is a note in the DRV8301 datasheet that says: "PWM with three independent inputs. PWM control high side gates only. Low side is complementary to high side gates with minimum...
    on Feb 27, 2012
  • Forum Post: Re: DRV8301/2 dead time setting in 3-input mode.

    Shane Colton Shane Colton
    Okay, thanks. I interpreted that as saying that external dead time set by the microcontroller (on INH and INL pins) would be observed as long as it was longer than the DTC resistor setting. So, if there was a 1us gap between INH high-to-low transistion and INL low-to-high transition, it would override...
    on Feb 27, 2012
  • Forum Post: Re: DRV8301/2 dead time setting in 3-input mode.

    Shane Colton Shane Colton
    Thank you, question answered!
    on Feb 28, 2012
  • Forum Post: How can I read the fault from the status registers in the DRV8301?

    Jason Work Jason Work
    I am having some difficulty reading the fault from the status registers of the DRV8301, and I'm looking for some guidance. Here is my setup: Code Composer Studio version 5.2.1.00018 controlSUITE v3.0.0 Hardware: DRV8301-HC-C2-KIT (DRV8301-HC-RevC1-RELEASE.pdf) with TMDSCNCD28035ISO controlCARD...
    on Jul 19, 2012
  • Forum Post: DRV8301 high power

    Rachel Coulter Rachel Coulter
    Does TI have any app notes/reference designs that would be applicable to higher power (100-1500W) level motor drive designs for the DRV8301? Thanks, Rachel
    on Aug 31, 2012
  • Forum Post: RE: DRV8301 3 phase pre driver with Integrated Buck Regulator

    SUnderwood1 SUnderwood1
    Ok Great. The DRV8301 data sheet block diagram indicates the buck regulator power input (PVDD2) is completely independent from the motor driver power in (PVDD1). So I can run the buck regulator on PVDD2 with the rest of the driver unpowered (PVDD1) ? correct? Is there any issue if the buck regulator...
    on Oct 31, 2012
  • Forum Post: DRV8301 Questions...

    David Petticord David Petticord
    We have a motor controller design based on the DRV8301 and an Atmel uC . It works as expected for supply voltages below 30 volts. However when we try to drive a motor with 36 volts it goes into fault lockups (intermittently). Up until now we have been using the default settings (no need to use...
    on Nov 19, 2012
  • Forum Post: DRV8301 - 4 quadrant control

    Matthias Stark1 Matthias Stark1
    Hi! Which TI motor drivers can be used to realize four-quadrant control of permanent magnet/brushless motors? In particular, it would be interesting if the DRV8301 could be used for that application?! Thanks a lot!
    on Jan 8, 2013
  • Forum Post: DRV8301 PVDD max voltage ramp rate

    Derek King1 Derek King1
    According to the datasheet the max PVDD ramp rate is 50V/ms. It also specifies that PVDD1 is completely independent of PVDD2. In a another post it is explained that a faster voltage ramp will cause logic problems, but not damage . http://e2e.ti.com/support/applications/motor_drivers/f/38/p/200671/849287...
    on Apr 3, 2013
  • Forum Post: DRV8301 Gate driver loading Qg(TOT)

    Derek King1 Derek King1
    The datasheet for the DRV8301 states the gate driver "Support up to 200kHz switching frequency with Qg(TOT)=25nC or total 30mA gate drive average current". In this statement, what is Qg(TOT)? 1. The Qg for a single FET? At 200kHz each highside and lowside FET can have a Qg of 25nC. 2...
    on Apr 3, 2013
  • Forum Post: multiple BLDC motor system with DRV8301s

    Pete Owen Pete Owen
    Hello, I recently completed a test that required control of eight BLDC motors (48V/5A/10k RPM) using eight DRV8301-HC-C2-KIT eval boards running lightly modified Instaspin software and a Stellaris Launchpad to control them all over SPI. This worked well, but required a huge box, so the next stage of...
    on Apr 10, 2013
  • Forum Post: BLDC motor control basics using DRV8312/8313 and an MSP430/Arduino

    Sashwat Mahapatra Sashwat Mahapatra
    Hi, I am just getting my hands into brushless DC motor control. I have the Exceed RC legend Motor 2402-2350KV motor (Links provided below). I need to learn how to control it. Can you help me get started? I have samples of the DRV8312, DRV8313, and the DRV 8301 ICs. I also have Arduino nano, Due, and...
    on May 14, 2013
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use