Other Parts Discussed in Thread: TIDA-00168, ADS1220
I want to use a T-type thermocouple with the TIDA-00650 reference board. I am using TIDA-00168 example code. I changed to a T-type connector and changed the PGA gain to 64 considering max voltage at 400C is 20.872 mV. Do I need to change filter/biasing circuits to accomodate the change? I am getting a wrong reading with this setup.
Thanks!