Part Number: PMP4311
I am evaluating a PMP4311 design for 5KW PFC. The design difference is that I am using the boost inductance value to be half of what is mentioned in the BOM. Now the trouble is the output stabilises at 380Vrms on 'NO LOAD', but as soon as I apply a nominal load i.e. about 200Ohm approximately 2 A of load current; the output voltage drops to about 300V. I can see the switching pulse of gate driver on an Oscilloscope. The input is 230VAC at 50 Hz. Any suggestion as to what the issue might be ?