This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00195: Transformer (T2,T3,T4) part number in TIDA-00195 (IGBT Gate Driver Evaluation Platform for 3-Phase Inverter System) design

Part Number: TIDA-00195

Hi folks,

I am using the TIDA-00195 reference design ( IGBT Gate Driver Evaluation Platform for 3-Phase Inverter System) IM application. With this design, the BOM was also included in the file. In the BOM, all the components are available from the respective vendors except a transformer (T2,T3,T4 in TIDA-00195) from Wurth Electronik. This transformer is neither available with vendor nor other suppliers. Please help me with the component details or alternative / equivalent to the existing component. I am also disclosing the part number & make of the transformer. 

Transformer

Part Number :750342573

Make : Wurth Elektronik