This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TIDA-00476: TIDA-00476 search for some files

Part Number: TIDA-00476

I want to use the reference design TIDA-00476.
This is my first attemp to work with the MSP430F5132IDAR controller.

For my use I need to change something in the software but I can't find some files
like driver.c etc.  Are these files in the TIDA-00476_LIBR.lib  file?

For example, I want to have the load switched at 1.5V and I need to added a I2c real time clock.

thanks in advance,

Rob Keij

  • Hello Rob,

    I am going to reach out to our TI Design team to look into how to help you. As many TIers are on vacation for the holidays, a response may be a little delayed. In the meantime, there are great example codes for the MSP430F5132 to help you implement I2C communication and other peripherals in our Resource Explorer. Thank you for your patience.

    Best regards,

    Matt Calvo

  • Hi,

    Yes the files are packaged into the TIDA-00476_LIBR.lib. If you need the source files, please reach out through TI sales channel and I will be share them with you.

    Best Regards,

    Ram

  • In reply to Ramkumar S:

    Hello Ramkumar,

    Thanks for the Quick reply I'm going to contact via TI sales channel.

    regards,

    Rob

  • In reply to Ramkumar S:

    20171231_SolarRegulator.pdf

    Dear Ramkumar,

    I have already designed the new print and have had to move some pins because I also need I2C for the RTC.
    My only supplier which the MSP430F5132IDAR has sufficient stock is mouser.
    So I try to request the missing source files via them, but until now I only received a quotation for 1 controller :)? .
    possibly that the seller had misunderstood my question .....

    I hope to have these missing files quickly so that I do not have to spend too much time writing software that is actually already available.

    maybe it possible to email the files directly : rob.keij@spi-electronics.nl

    I include the schematic with the RTC (I change the schematic to a clear one pager )


    thanks in advance,

    Best regards,

    Rob Keij

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.