This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EV-LM3S811 blinking LED in assembler

Intellectual 450 points

Replies: 4

Views: 3875

For the really hard core folk that want to get to the bare metal of the new Stellaris parts, here is a minimal program that will blink the user LED on the EV-LM3S811 board, in glorious ARM assembler code, which will compile under the uVision demo that is supplied with the evaluation kit:

; blink.s - blink user LED on Luminary Micro EV-LM3S811 (Cortex-M3)

AREA TEXT, CODE, READONLY
CODE16

; vector table

DCD 0x20002000
DCD Reset_Handler
DCD iloop
DCD iloop

; start the program here

Reset_Handler
EXPORT Reset_Handler

; initialize GPIO port C, pin 5 as output

RCGC2 EQU 0x400FE108 ; run-mode clock gating control 2
RCGC2_PORTC EQU 1 <

ldr r0, =RCGC2

ldr r1, =RCGC2_PORTC
str r1, [r0]

GPIODIR_PORTC EQU 0x40006400
GPIO_PC5 EQU 1 <

ldr r0, =GPIODIR_PORTC

ldr r1, =GPIO_PC5
str r1, [r0]

GPIODATA_PORTC EQU 0x40006000

ldr r0, =GPIODATA_PORTC + (GPIO_PC5 <

loop

ldr r1, =GPIO_PC5
str r1, [r0]

ldr r2, =1000000
1 subs r2, r2, #1
bne %1

ldr r1, =0
str r1, [r0]

ldr r2, =1000000
1 subs r2, r2, #1
bne %1

b loop ; and do it again

; an infinite loop in place of real exception handlers

iloop b iloop

; the end

END

[end-of-file]

Note that you will need to indent all the lines that don't start with a label, as this forum is protecting you from my code in its original beauty.

Questions? Comments? Let me know!

Dale

4 Replies

  • Thanks for the example! I want to experiment with asm a little more.

    I think you can use the "Code" button on the web page here to tell it not to mess up your indenting. When entering code in a message, try highlighting the code and then press the code button.

    Here's a test - I want to see if this works:

    Code:


     comment not indented
    label
    :     ; not indented
      code1    
    indented 2 spaces
        code2  
    indented 4 spaces
    lable2
    :    ; not indented



  • Oh, that's much better! Let me try this again, using the appropriate tools this time:

    Code:


     blink.blink user LED on Luminary Micro EV-LM3S811 (Cortex-M3)

        
    AREA    TEXTCODEREADONLY
        CODE16

        
    vector table

        DCD    0x20002000
        DCD    Reset_Handler
        DCD    iloop
        DCD    iloop

        
    start the program here

    Reset_Handler
        EXPORT Reset_Handler

        
    initialize GPIO port Cpin 5 as output

    RCGC2            EQU 0x400FE108        
    run-mode clock gating control 2
    RCGC2_PORTC        EQU 1 
    <2            PORTC clock enable

        ldr    r0
    , =RCGC2

        ldr    r1
    , =RCGC2_PORTC
        str    r1
    , [r0]

    GPIODIR_PORTC    EQU 0x40006400
    GPIO_PC5        EQU 1 
    <5

        ldr    r0
    , =GPIODIR_PORTC
        
        ldr    r1
    , =GPIO_PC5
        str    r1
    , [r0]

    GPIODATA_PORTC    EQU 0x40006000

        ldr    r0
    , =GPIODATA_PORTC + (GPIO_PC5 <2)

    loop
        
        ldr    r1
    , =GPIO_PC5
        str    r1
    , [r0]

        
    ldr    r2, =1000000
    1    subs    r2
    r2#1
        
    bne    %1

        ldr    r1
    , =0
        str    r1
    , [r0]
        
        
    ldr    r2, =1000000
    1    subs    r2
    r2#1
        
    bne    %1

        b    loop    
    ; and do it again

        
    an infinite loop in place of real exception handlers

    iloop    b    iloop

        
    the end

        END

    [end-of-file]






    Awesome! You might actually be able to cut+paste and get it to work! Thanks for the tip.

    Dale
  • Dale,

    Thanks for posting the code. Do you have any extra ASM to switch clocks to run the CPU at 50 MHz?

    Out of interest, I created a very simple 'blinky' program in C using RV3 running the CPU at 50 MHz (SYSDIV _4) - the fastest I could get it to go using the LM Library calls was 541 KHz! Hence my request for ASM code to set the PLL.

    Pete
  • This looks interesting - but how does one set up an Assembler project in code_suite?

    The documentation seems to be entirely focussed on C/C++...

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.