Additive Synthesizer w/ GUI

Microcomputer System 1 (ECE-3551)
Dr. Veton Kepuska
Florida Institute of Technology


Overview

Project Title: Additive Synthesizer with GUI

Author: Yordan Lasonov

Year: 2011

Description: 

For the final project, the board was used for creating an additive synthesizer. The synthesizer parameters
were mapped to GUI (graphic user interface) created in Visual Basic. In order to facilitate user input music
keys, the keyboard was used via serial port.


 


Files Included
  • C Code for DM6437
  • Project Report and Presentation
Related
Recommended