Keyboard Equalization Controller

Microcomputer Systems I (ECE-3551)
Dr. Veton Kepuska
Florida Institute of Technology, Melbourne FL


Overview

Author: Talles Tatagiba Martins de Souza
Date: Fall 2012
Description:

For my final project, my goal was to create a micro-controller interface to communicate with the DSP in order to do Equalization. For already stated reasons, there was an issue in the original project that made it impossible to complete, so the project was rapidly changed in order to use the keyboard as input to make the Equalization. Equalization is the process of adjusting the balance between frequency components within an electronic signal, which is in our case, a sound.

The main purpose of the project was to become more familiarized with Universal asynchronous receiver/transmitter and the Fast-Fourier Transform Algorithm and its applications.


Files Included

  • C Code for DM6437
  • Project Report and Presentation
Related
Recommended