Hi, I am using Jacinto 6, GLSDK 7.04.03.
If we replace eMMC to "N25Q064A13E12H0F" on DRA742-EVM 577G-02-21-00 board, should i modify any code?
As i see in dra7-evm.dts file, there are description about QSPI like below
&qspi {
status = "okay";
spi-max-frequency = <64000000>;
m25p80@0 {
compatible = "s25fl256s1";
spi-max-frequency = <64000000>;
the value of compatible is the original QSPI flash, so i think i should modify here, am i right?
besides, is there any place should i modify too?