This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

Not able to access EMIF2 : DDR3L

Hi

We are using X5777BXGABC processor in one of our design.Where I'm not able to access DDR3L chips(1GB) which has connected to the EMIF2 controller.

I tried connecting JTAG with reduced clock but not able to access any of the DDR registers.

One thing i could observe by probing is that CKE of EMIF2 is not toggling.Its idle  as high(Vtt).

Can any one help me further debugging this issue.

  • Hi Anand,

    I have forwarded your question to EMIF experts to help.
    Meanwhile you can check if you can find something useful in this document:
    www.ti.com/.../sprac36.pdf

    Regards,
    Yordan
  • In reply to Yordan Kamenov:

    Hi Anand,

    Please check if the CTRL_CORE_SMA_SW_0[1] EMIF2_CKE_GATING_CTRL bit is cleared. If set to 0x1, EMIF2 can't take control over CKE.
    I assume everything is fine with EMIF1. If you also have 1GB connected to EMIF1, you can use the same register settings for EMIF2. The only difference is that EMIF2 doesn't support ECC.

    Another thing to check are the DMM_LISA_MAP_i, the CTRL_WKUP_SECURE_EMIF2_SDRAM_CONFIG and CTRL_WKUP_EMIF2_SDRAM_CONFIG_EXT registers.

    BR,
    Dobrin

     Please click the Verify Answer button on this post if it answers your question.

       Please make sure you read the forum guidelines first.

  • In reply to Dobrin Dobrinov:

    Dear Dobrin,

    Thanks for the reply,

    I have tried reading the register CTRL_CORE_SMA_SW_0
    EMIF2_CKE_GATING_CTRL bit set 0x0.So its clear that CKE pad controlled by processor.

    Your assumption is correct ,I do have DDR3L chips connected to EMIF1 controller and its working fine.The same registers setting i used for EMIF2 but there is no improvements.

    One more observation,I have connected JTAG debugger with configuration setting only EMIF2.I'm able to write on some of the DDR address locations but the data on adjacent locations also getting affected.
  • In reply to Anand Ram Karanth:

    Anand,

    Have you also checked the control module registers? The CTRL_WKUP_SECURE_EMIF2_SDRAM_CONFIG register exports its values to EMIF2.EMIF_SDRAM_CONFIG register at POR. CTRL_WKUP_SECURE_EMIF2_SDRAM_CONFIG should have same settings as CTRL_WKUP_SECURE_EMIF1_SDRAM_CONFIG register. These registers are used to specify important EMIF parameters.

    The CTRL_WKUP_EMIF2_SDRAM_CONFIG_EXT register should also have same values as CTRL_WKUP_EMIF1_SDRAM_CONFIG_EXT (assuming you don't use ECC, otherwise ECC must be enabled in CTRL_WKUP_EMIF1_SDRAM_CONFIG_EXT).

    The DMM_LISA_MAP_i registers are also important. They control the interleaving between EMIF1 and EMIF2, address mapping and other important parameters. There are also registers that control the output impedance, slew rate and weak pull resistors of the DDR IO cells. These regs are: CTRL_CORE_CONTROL_DDRCACH1_0, CTRL_CORE_CONTROL_DDRCH1_0, CTRL_CORE_CONTROL_DDRCH1_1, CTRL_CORE_CONTROL_DDRCH1_2 for EMIF1 and CTRL_CORE_CONTROL_DDRCACH2_0, CTRL_CORE_CONTROL_DDRCH2_0, CTRL_CORE_CONTROL_DDRCH2_1 for EMIF2.

    In addition, when you use JTAG, do you use CCS and default gel files? The EMIF gel file performs all required steps to initialize both EMIFs.

    One more question, I assume your board is designed using fly-by topology and leveling, right?

    BR,
    Dobrin

     Please click the Verify Answer button on this post if it answers your question.

       Please make sure you read the forum guidelines first.

  • In reply to Dobrin Dobrinov:

    Dobrin,

    I have checked all the registers parameters values as you mentioned earlier for EMIF1 and EMIF2.
    We observed that the values are same for the both EMIF's registers as we are configuring from the Uboot code.

    Also we tried with the available gel file (/opt/ti/ccv5/ccs_base/emullation/gel/DRAxx/DRA7xx_ddr_config.gel) with the modified value in lisa_map register. We are not able to access the EMIF2 memory controller's DDR.

    We thought to debug from the hardware side and we have observed that CKE is not toggling for EMIF2 controller and the signal is always high.


    Regards
    Anand
  • In reply to Anand Ram Karanth:

    Anand,

    I also thought about HW issue but first wanted to confirm everything is OK from SW side.

    High level of CKE is normal. According to DDR3 JEDEC spec (JESD79-3F) CKE is low only during Self Refresh and Power Down commands. It must be high during reads and writes. Here is an excerpt:

    Could you please send the LISA_MAP_i register settings just to verify everything is OK?

    BR,

    Dobrin


     Please click the Verify Answer button on this post if it answers your question.

       Please make sure you read the forum guidelines first.

  • In reply to Dobrin Dobrinov:

    Hi Dobrin,

    Please find below LISA_MAP_i register settings that we have configured for 1.5GB.

    .dmm_lisa_map_0 = 0x0

    .dmm_lisa_map_1 = 0x80640300

    .dmm_lisa_map_2 = 0xc0500220

    .dmm_lisa_map_3 = 0xff020100

    I have one more doubt regarding CKE signal voltage level.The Vih(min) level should be more than Vref correct?
    In our scenario its exactly VDDQ/2.
  • In reply to Anand Ram Karanth:

    Anand,

    Sorry for the late reply… According to the J6 data manual Voh min of CKE is 0,9*VDDS, and VREF is 0,5*VDDS. Obviously, Voh min of CKE must be more than VREF. Have you compared EMIF1 CKE and EMIF2 CKE?

    The LISA_MAP settings seem to be OK. You have 1,5GB configuration. 1GB interleaved between EMIF1 and EMIF2 with 256b granularity and 512MB mapped only to EMIF1.

    BR,
    Dobrin

     Please click the Verify Answer button on this post if it answers your question.

       Please make sure you read the forum guidelines first.

  • In reply to Dobrin Dobrinov:

    Dobrin,

    Yes I have compared CKE of working EMIF1 and Its toggling during initialization stage(going low then high) but same thing not happening on other EMIF2 CKE signal.

    So, testing purpose I have shorted CKE of EMIF1 to EMIF2 CKE and my board booted successfully.I tried with both 1.5GB and 2GB configuration and Its working fine.

    I would like to know whether this approach is fine ?

    Regards
    Anand
  • In reply to Anand Ram Karanth:

    Anand,

    It seems to be a HW issue with EMIF2 CKE. Have you measured the termination resistor between CKE and VTT? It should have same value as the one for EMIF1. Do you have pull down connected to CKE? Please check.

    It's not a good approach to short EMIF1 and EMIF2 CKE signals. IMO, the board has booted successfully not because you have connected EMIF2 CKE to EMIF1 CKE but because you have connected it to a valid voltage level. If you had connected EMIF2 CKE to another valid voltage level that remains high, you shall also have booted successfully. As I previously said, CKE is low only during Self Refresh and Power Down commands.

    Please check the resistor values as I mentioned above.

    BR,
    Dobrin

     Please click the Verify Answer button on this post if it answers your question.

       Please make sure you read the forum guidelines first.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.