Other Parts Discussed in Thread: DRA752
Hello.
I just upgraded to RadioApp (RA) 1.50.21.01 from 1.50.20.02. I am running 6AM.1.3. I replaced all the prebuilts on the device with the ones from the 21.01 distribution.
(With the exception of cmem - we compiled that one directly from the 6AM.1.3 source, to match the kernel (had to do the same when using 20.02).
I can no longer successfully tune radio stations (JAMR3) using Dracon (the version included with 1.50.21.01), or my own simple Android socket client app.
My company has a custom RA_1.50.20.02 from TI that resolved a garbled audio issue. 1.50.21.01 was expected to work without modification.
I suspect I just need to dial in the command line options - I see that there are new options in 21.01.
With 20.02, I started the app:
RadioApp -h eth -o ARM -a 127.0.0.1
I did not background it, so I could see the messages.
My clients (Dracon included) run on the board, and connect to 127.0.0.1/3125. I use TUNER_ONBOARD, and '
RM_HDMRC_SD_CUNCURRENCY_EN' (14) (I don't get HD coverage in my area - this concurrency allows me to at least get static).
With the above options, Dracon hangs after the 'Connected!' log message. Similarly for 'RadioApp -h eth -o ARM -t 0 -a 127.0.0.1'.
I also tried
'RadioApp -h eth -h cli -t 0 -a 127.0.0.1'
and the commands 'tunerselect onboard 14` (which responded '
SV: SV_RADIO_SELECT_TUNER') followed by
'radioband 0 FM' and 'radiotune 0 98.1', which responded 'Waiting for the acknowledgment of previous user command'
Finally:
'RadioApp -o ARM -h cli -h eth -a 127.0.0.1 -t 1 -l 1 -u 14'
That configuration never gives me a 'CLI>'
As a first step, please let me know which command line options I should use, then, let me know what other information you might need.
-Thanks
-Greg