Part Number: DRA72XEVM
Tool/software: TI-RTOS
when i use the ti driver components of M4, following error happened,
1、config the opmode UART_OPMODE_DMAINTERRUPT
2、config the event enable
3、send and receive messages in period task
4、debug my program,use the logic analyzer to read if the messages is right or not
what i found is that, the m4 was always sending 56 bytes “\0”,which is equal to txThreshold,and always receiving 8 bytes “\0”,which is equal to rxThreshold。
but actually,what i wanted to send is 0x01, 0x02....and receive is 0x01,0x02 in my program.
i checked the program , can't find the reason.
Is there someone have met the same thing as me? how can i solve this problem?
ps:when i config the opmode UART_OPMODE_INTERRUPT, it worked very well.