Our processor is DRA71X and DRA74X, with 3.02.00.03 SDK version.
We want to test SATA interface through access SSD device(Apacer APM2T42P100008GAN-GTM1).
1.Does 3.02.00.03 SDK support SATA operation(read/write) on this ssd device?
2.If the answer of question-1 is yes, Does system will automatically probe this ssd device or i've to add description for it at dts file?
3.How could i access this device? Like normally device operation(i.e. ls /dev/xxx) or need some special command to do it?
P.S. the ssd device product info link as follow =>
Regards,
Shawn