Our processor is DRA74X, with 3.02.00.03 SDK version.
At our custom board, there is video converter(ADV7611), and it's 8-bit BT656 output directly connect to Vin-3a port of DRA74X. And DRA74X use i2c-1 to control this converter.
I already modify dts file to make a connection between vin3a & ADV7611. I can see /dev/video1 by " ls /dev/video* ", but after i use " v4l2-ctl --list-device ", there is no /dev/video1.
I also try to open it at my AP program, still fail. What is the possible reson to cause this?
Here is the boot log =>
U-Boot SPL 2016.05-g9694c57-dirty (Jul 06 2018 - 16:04:55) DRA752-GP ES2.0 no pinctrl for hs200_1_8v no pinctrl for ddr_1_8v @SD max clock = 10000000@ *** Warning - bad CRC, using default environment Trying to boot from MMC1 *** Warning - bad CRC, using default environment reading u-boot.img reading u-boot.img reading u-boot.img reading u-boot.img U-Boot 2016.05-g9694c57-dirty (Jul 06 2018 - 16:04:55 +0800) CPU : DRA752-GP ES2.0 Model: TI DRA742 Board: DRA74x EVM REV DRAM: 2 GiB NAND: 256 MiB MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1 *** Warning - bad CRC, using default environment current ID is 7 Warning: fastboot.board_rev: unknown board revision GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645 part_get_info_efi: *** ERROR: Invalid GPT *** GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645 part_get_info_efi: *** ERROR: Invalid Backup GPT *** ERROR: cannot find partition: 'userdata' at arch/arm/cpu/armv7/omap-common/utils.c:199/mmc_get_part_size() Warning: fastboot.userdata_size: unable to calc SCSI: SATA link 0 timeout. AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst scanning bus for devices... Found 0 device(s). Net: Warning: ethernet@48484000 using MAC address from ROM eth0: ethernet@48484000 Hit any key to stop autoboot: 0 load MAN2020_original.dtb load MAN2020_3g switch to partitions #0, OK mmc0 is current device @SD max clock = 10000000@ SD/MMC found on device 0 reading boot.scr ** Unable to read file boot.scr ** reading uEnv.txt 222 bytes read in 3 ms (72.3 KiB/s) Loaded env from uEnv.txt Importing environment from mmc0 ... @SD max clock = 10000000@ switch to partitions #0, OK mmc0 is current device @SD max clock = 10000000@ SD/MMC found on device 0 3651816 bytes read in 785 ms (4.4 MiB/s) 112109 bytes read in 86 ms (1.2 MiB/s) Booting from mmc0 ... Kernel image @ 0x82000000 [ 0x000000 - 0x37b8e8 ] ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Loading Device Tree to 8ffe1000, end 8ffff5ec ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Initializing cgroup subsys cpuset [ 0.000000] Initializing cgroup subsys cpu [ 0.000000] Initializing cgroup subsys cpuacct [ 0.000000] Linux version 4.4.45-g0422030-dirty (hsuyz@hsuyz-VirtualBox) (gcc version 5.3.1 20160113 (Linaro GCC 5.3-2016.02) ) #55 SMP PREEMPT Fri Jul 6 16:05:16 CST 2018 [ 0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=30c5387d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache [ 0.000000] Machine model: TI DRA742 [ 0.000000] cma: Reserved 64 MiB at 0x00000000fac00000 [ 0.000000] Forcing write-allocate cache policy for SMP [ 0.000000] Memory policy: Data cache writealloc [ 0.000000] DRA752 ES2.0 [ 0.000000] PERCPU: Embedded 11 pages/cpu @eed9f000 s14848 r8192 d22016 u45056 [ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 517952 [ 0.000000] Kernel command line: console=ttyO3,115200n8 elevator=noop root=/dev/mmcblk0p2 rw rootwait earlyprintk fixrtc omapdrm.num_crtc=2 consoleblank=0 cma=64M rootfstype=ext4 snd.slots_reserved=1,1 [ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes) [ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes) [ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes) [ 0.000000] Memory: 1983276K/2078720K available (6663K kernel code, 364K rwdata, 2500K rodata, 336K init, 302K bss, 29908K reserved, 65536K cma-reserved, 1226752K highmem) [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB) [ 0.000000] vmalloc : 0xf0800000 - 0xff800000 ( 240 MB) [ 0.000000] lowmem : 0xc0000000 - 0xf0000000 ( 768 MB) [ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB) [ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB) [ 0.000000] .text : 0xc0008000 - 0xc08fb09c (9165 kB) [ 0.000000] .init : 0xc08fc000 - 0xc0950000 ( 336 kB) [ 0.000000] .data : 0xc0950000 - 0xc09ab390 ( 365 kB) [ 0.000000] .bss : 0xc09ad000 - 0xc09f8a78 ( 303 kB) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1 [ 0.000000] Preemptible hierarchical RCU implementation. [ 0.000000] Build-time adjustment of leaf fanout to 32. [ 0.000000] NR_IRQS:16 nr_irqs:16 16 [ 0.000000] ti_dt_clocks_register: failed to lookup clock node gmac_gmii_ref_clk_div [ 0.000000] OMAP clockevent source: timer1 at 31475 Hz [ 0.000000] Architected cp15 timer(s) running at 5.90MHz (phys). [ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x15c70fb29, max_idle_ns: 440795202138 ns [ 0.000004] sched_clock: 56 bits at 5MHz, resolution 169ns, wraps every 4398046511093ns [ 0.000016] Switching to timer-based delay loop, resolution 169ns [ 0.000331] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns [ 0.000339] OMAP clocksource: 32k_counter at 32768 Hz [ 0.000793] Console: colour dummy device 80x30 [ 0.000810] WARNING: Your 'console=ttyO3' has been replaced by 'ttyS3' [ 0.000817] This ensures that you still see kernel messages. Please [ 0.000822] update your kernel commandline. [ 0.000835] Calibrating delay loop (skipped), value calculated using timer frequency.. 11.80 BogoMIPS (lpj=59016) [ 0.000847] pid_max: default: 32768 minimum: 301 [ 0.000941] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes) [ 0.000952] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes) [ 0.001531] Initializing cgroup subsys io [ 0.001548] Initializing cgroup subsys memory [ 0.001573] Initializing cgroup subsys devices [ 0.001585] Initializing cgroup subsys freezer [ 0.001597] Initializing cgroup subsys perf_event [ 0.001608] Initializing cgroup subsys pids [ 0.001634] CPU: Testing write buffer coherency: ok [ 0.001845] /cpus/cpu@0 missing clock-frequency property [ 0.001862] /cpus/cpu@1 missing clock-frequency property [ 0.001872] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000 [ 0.001909] Setting up static identity map for 0x800082c0 - 0x80008320 [ 0.080107] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001 [ 0.080169] Brought up 2 CPUs [ 0.080183] SMP: Total of 2 processors activated (23.60 BogoMIPS). [ 0.080189] CPU: All CPU(s) started in HYP mode. [ 0.080195] CPU: Virtualization extensions available. [ 0.080579] devtmpfs: initialized [ 0.110989] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0 [ 0.111991] omap_hwmod: l3_main_2 using broken dt data from ocp [ 0.309786] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns [ 0.311303] pinctrl core: initialized pinctrl subsystem [ 0.312153] NET: Registered protocol family 16 [ 0.313148] DMA: preallocated 256 KiB pool for atomic coherent allocations [ 0.340224] cpuidle: using governor ladder [ 0.370249] cpuidle: using governor menu [ 0.378547] OMAP GPIO hardware version 0.1 [ 0.382666] GPIO line 161 (radio_rst) hogged as output/low [ 0.385006] irq: no irq domain found for /ocp/l4@4a000000/scm@2000/pinmux@1400 ! [ 0.401836] omap-gpmc 50000000.gpmc: GPMC revision 6.0 [ 0.401849] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000 [ 0.412006] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers. [ 0.412016] hw-breakpoint: maximum watchpoint size is 8 bytes. [ 0.412815] OMAP DMA hardware revision 0.0 [ 0.451884] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver (LinkedList1/2/3 supported) [ 0.453059] edma 43300000.edma: memcpy is disabled [ 0.457801] edma 43300000.edma: TI EDMA DMA engine driver [ 0.464792] palmas 0-0058: IRQ missing: skipping irq request [ 0.481476] palmas 0-0058: Muxing GPIO a, PWM 0, LED 0 [ 0.481597] @@@@1 [ 0.481815] @@@@3 [ 0.481827] @@@@4 [ 0.481836] @@@@5 [ 0.482191] @@@@6 [ 0.482354] @@@@7 [ 0.491128] @@@@8 [ 0.553168] @@@@9(0) [ 0.553185] @@@@2 [ 0.553332] omap_i2c 48070000.i2c: bus 0 rev0.12 at 400 kHz [ 0.553760] omap_i2c 48072000.i2c: bus 1 rev0.12 at 400 kHz [ 0.554124] omap_i2c 48060000.i2c: bus 2 rev0.12 at 400 kHz [ 0.554483] omap_i2c 4807a000.i2c: bus 3 rev0.12 at 400 kHz [ 0.554843] omap_i2c 4807c000.i2c: bus 4 rev0.12 at 400 kHz [ 0.555038] media: Linux media interface: v0.10 [ 0.555088] Linux video capture interface: v2.00 [ 0.555126] pps_core: LinuxPPS API ver. 1 registered [ 0.555133] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it> [ 0.555155] PTP clock support registered [ 0.555201] EDAC MC: Ver: 3.0.0 [ 0.556001] Advanced Linux Sound Architecture Driver Initialized. [ 0.556902] clocksource: Switched to clocksource arch_sys_counter [ 0.567620] NET: Registered protocol family 2 [ 0.568120] TCP established hash table entries: 8192 (order: 3, 32768 bytes) [ 0.568183] TCP bind hash table entries: 8192 (order: 4, 65536 bytes) [ 0.568308] TCP: Hash tables configured (established 8192 bind 8192) [ 0.568364] UDP hash table entries: 512 (order: 2, 16384 bytes) [ 0.568394] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes) [ 0.568610] NET: Registered protocol family 1 [ 0.568852] RPC: Registered named UNIX socket transport module. [ 0.568861] RPC: Registered udp transport module. [ 0.568868] RPC: Registered tcp transport module. [ 0.568874] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.569938] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available [ 0.572609] futex hash table entries: 512 (order: 3, 32768 bytes) [ 0.580361] squashfs: version 4.0 (2009/01/31) Phillip Lougher [ 0.581030] NFS: Registering the id_resolver key type [ 0.581057] Key type id_resolver registered [ 0.581065] Key type id_legacy registered [ 0.581129] ntfs: driver 2.1.32 [Flags: R/O]. [ 0.583108] bounce: pool size: 64 pages [ 0.583270] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 247) [ 0.583287] io scheduler noop registered (default) [ 0.583299] io scheduler deadline registered [ 0.583334] io scheduler cfq registered [ 0.588674] pinctrl-single 4a003400.pinmux: 282 pins at pa fc003400 size 1128 [ 0.652247] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled [ 0.655691] 4806a000.serial: ttyS0 at MMIO 0x4806a000 (irq = 299, base_baud = 3000000) is a 8250 [ 0.656578] 4806c000.serial: ttyS1 at MMIO 0x4806c000 (irq = 300, base_baud = 3000000) is a 8250 [ 0.657475] 48020000.serial: ttyS2 at MMIO 0x48020000 (irq = 301, base_baud = 3000000) is a 8250 [ 0.658307] console [ttyS3] disabled [ 0.658353] 4806e000.serial: ttyS3 at MMIO 0x4806e000 (irq = 302, base_baud = 3000000) is a 8250 [ 1.459438] console [ttyS3] enabled [ 1.463793] 48066000.serial: ttyS4 at MMIO 0x48066000 (irq = 303, base_baud = 3000000) is a 8250 [ 1.473446] 48422000.serial: ttyS7 at MMIO 0x48422000 (irq = 304, base_baud = 3000000) is a 8250 [ 1.483097] 48424000.serial: ttyS8 at MMIO 0x48424000 (irq = 305, base_baud = 3000000) is a 8250 [ 1.492754] 4ae2b000.serial: ttyS9 at MMIO 0x4ae2b000 (irq = 306, base_baud = 3000000) is a 8250 [ 1.502838] [drm] Initialized drm 1.1.0 20060810 [ 1.508943] OMAP DSS rev 6.1 [ 1.512715] omapdss_dss 58000000.dss: bound 58001000.dispc (ops dispc_component_ops) [ 1.528812] loop: module loaded [ 1.532822] nand: No NAND device found [ 1.536594] omap2-nand 8000000.nand: scan failed, may be bus-width mismatch [ 1.549059] m25p80 spi32766.0: s25fl256s1 (32768 Kbytes) [ 1.554454] 7 ofpart partitions found on MTD device spi32766.0 [ 1.560334] Creating 7 MTD partitions on "spi32766.0": [ 1.565497] 0x000000000000-0x000000040000 : "QSPI.MLO" [ 1.571581] 0x000000040000-0x000000140000 : "QSPI.u-boot" [ 1.577890] 0x000000140000-0x0000001c0000 : "QSPI.DRA7-evm.dtb" [ 1.584711] 0x0000001c0000-0x0000001d0000 : "QSPI.u-boot-env" [ 1.591368] 0x0000001d0000-0x0000001e0000 : "QSPI.u-boot-env.backup1" [ 1.598723] 0x0000001e0000-0x0000009e0000 : "QSPI.uImage" [ 1.604975] 0x0000009e0000-0x000002000000 : "QSPI.IPU-exe" [ 1.612361] libphy: Fixed MDIO Bus: probed [ 1.617077] CAN device driver interface [ 1.621301] pinctrl-single 4a003400.pinmux: pin 4a003818.0 already requested by 4a003400.pinmux; cannot claim for 4ae3c000.can [ 1.632761] pinctrl-single 4a003400.pinmux: pin-262 (4ae3c000.can) status -22 [ 1.639946] pinctrl-single 4a003400.pinmux: could not request pin 262 (4a003818.0) from group dcan1_pins_sleep on device pinctrl-single [ 1.652278] c_can_platform 4ae3c000.can: Error applying setting, reverse things back [ 1.660721] c_can_platform 4ae3c000.can: c_can_platform device registered (regs=fce3c000, irq=357) [ 1.716934] davinci_mdio 48485000.mdio: davinci mdio revision 1.6 [ 1.723059] libphy: 48485000.mdio: probed [ 1.727109] mdio_bus 48485000.mdio: /ocp/ethernet@48484000/mdio@48485000/micrel_phy_config has invalid PHY address [ 1.737519] mdio_bus 48485000.mdio: /ocp/ethernet@48484000/mdio@48485000/rmii-ref has invalid PHY address [ 1.747145] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 0 [ 1.756655] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 1 [ 1.764519] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 2 [ 1.772319] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 3 [ 1.780119] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 4 [ 1.789268] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 5 [ 1.797277] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 6 [ 1.805078] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 7 [ 1.812879] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 8 [ 1.820679] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 9 [ 1.828479] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 10 [ 1.836277] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 11 [ 1.844078] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 12 [ 1.851878] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 13 [ 1.859678] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 14 [ 1.867478] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 15 [ 1.875277] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 16 [ 1.883075] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 17 [ 1.890878] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 18 [ 1.898678] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 19 [ 1.906477] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 20 [ 1.914277] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 21 [ 1.922078] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 22 [ 1.929878] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 23 [ 1.937677] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 24 [ 1.945477] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 25 [ 1.953278] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 26 [ 1.961077] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 27 [ 1.968878] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 28 [ 1.976677] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 29 [ 1.984478] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 30 [ 1.992278] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 31 [ 2.000080] mdio_bus 48485000.mdio: scan phy rmii-ref at address 1 [ 2.006837] mdio_bus 48485000.mdio: scan phy rmii-ref at address 2 [ 2.013597] mdio_bus 48485000.mdio: scan phy rmii-ref at address 3 [ 2.020358] mdio_bus 48485000.mdio: scan phy rmii-ref at address 5 [ 2.027115] mdio_bus 48485000.mdio: scan phy rmii-ref at address 6 [ 2.033877] mdio_bus 48485000.mdio: scan phy rmii-ref at address 7 [ 2.041158] mdio_bus 48485000.mdio: scan phy rmii-ref at address 8 [ 2.047918] mdio_bus 48485000.mdio: scan phy rmii-ref at address 9 [ 2.054677] mdio_bus 48485000.mdio: scan phy rmii-ref at address 10 [ 2.061957] mdio_bus 48485000.mdio: scan phy rmii-ref at address 11 [ 2.069238] mdio_bus 48485000.mdio: scan phy rmii-ref at address 12 [ 2.076516] mdio_bus 48485000.mdio: scan phy rmii-ref at address 13 [ 2.083798] mdio_bus 48485000.mdio: scan phy rmii-ref at address 14 [ 2.091077] mdio_bus 48485000.mdio: scan phy rmii-ref at address 15 [ 2.098357] mdio_bus 48485000.mdio: scan phy rmii-ref at address 16 [ 2.105637] mdio_bus 48485000.mdio: scan phy rmii-ref at address 17 [ 2.112918] mdio_bus 48485000.mdio: scan phy rmii-ref at address 18 [ 2.120198] mdio_bus 48485000.mdio: scan phy rmii-ref at address 19 [ 2.127478] mdio_bus 48485000.mdio: scan phy rmii-ref at address 20 [ 2.134757] mdio_bus 48485000.mdio: scan phy rmii-ref at address 21 [ 2.142037] mdio_bus 48485000.mdio: scan phy rmii-ref at address 22 [ 2.149318] mdio_bus 48485000.mdio: scan phy rmii-ref at address 23 [ 2.156597] mdio_bus 48485000.mdio: scan phy rmii-ref at address 24 [ 2.163878] mdio_bus 48485000.mdio: scan phy rmii-ref at address 25 [ 2.171158] mdio_bus 48485000.mdio: scan phy rmii-ref at address 26 [ 2.178437] mdio_bus 48485000.mdio: scan phy rmii-ref at address 27 [ 2.185717] mdio_bus 48485000.mdio: scan phy rmii-ref at address 28 [ 2.192997] mdio_bus 48485000.mdio: scan phy rmii-ref at address 29 [ 2.200278] mdio_bus 48485000.mdio: scan phy rmii-ref at address 30 [ 2.207558] mdio_bus 48485000.mdio: scan phy rmii-ref at address 31 [ 2.214839] davinci_mdio 48485000.mdio: phy[0]: device 48485000.mdio:00, driver Micrel KSZ8081 or KSZ8091 [ 2.224462] davinci_mdio 48485000.mdio: phy[4]: device 48485000.mdio:04, driver Micrel KSZ8081 or KSZ8091 [ 2.234482] cpsw 48484000.ethernet: No slave[0] phy_id, phy-handle, or fixed-link property [ 2.242944] cpsw 48484000.ethernet: Detected MACID = f0:45:da:8a:80:e6 [ 2.249606] cpsw 48484000.ethernet: cpts: overflow check period 800 [ 2.257745] mousedev: PS/2 mouse device common for all mice [ 2.273954] i2c /dev entries driver [ 2.278247] @@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@ [ 2.283757] 11111111111111111111111@@@@@@@@@@@@@@@@@@@@@@@@ [ 2.289370] 22222222222222222222222@@@@@@@@@@@@@@@@@@@@@@@@ [ 2.294966] 3333333333333333333333333333@@@@@@@@@@@@@@@@@@@@@@@@ [ 2.301013] 44444444444444444444444444444@@@@@@@@@@@@@@@@@@@@@@@@ [ 2.307433] 55555555555555555555555555555@@@@@@@@@@@@@@@@@@@@@@@@ [ 2.313552] 8888888888888888888888888888888@@@@@@@@@@@@@ [ 2.354257] adv7611 0-004c: adv7611 found @ 0x98 (OMAP I2C adapter) [ 2.361469] vpe 489d0000.vpe: loading firmware vpdma-1b8.bin [ 2.368578] vip 48990000.vip: loading firmware vpdma-1b8.bin [ 2.378800] omap_hsmmc 4809c000.mmc: Got CD GPIO [ 2.387090] vpe 489d0000.vpe: Device registered as /dev/video0 [ 2.396925] vip 48990000.vip: VPDMA firmware loaded [ 2.401944] vip2-s0: Port A: Using subdev adv7611 0-004c for capture [ 2.408731] vip2-s0: device registered as video1 [ 2.427606] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr25 mode [ 2.433989] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr12 mode [ 2.440551] evm_3v3_sw: supplied by sysen1 [ 2.477283] omap_hsmmc 480ad000.mmc: no pinctrl state for sdr50 mode [ 2.483669] omap_hsmmc 480ad000.mmc: no pinctrl state for sdr25 mode [ 2.490066] omap_hsmmc 480ad000.mmc: no pinctrl state for sdr12 mode [ 2.496449] omap_hsmmc 480ad000.mmc: no pinctrl state for hs mode [ 2.537681] ledtrig-cpu: registered to indicate activity on CPUs [ 2.547876] hwspinlock_user gatemp: requested 10 hwspinlocks [ 2.554260] [ 2.554260] [spidrv_init] [ 2.558393] spidrv_init called [ 2.561469] [ 2.561469] [mcaspdrv_init] [ 2.565754] mcaspdrv_init called [ 2.570100] davinci-mcasp 48460000.mcasp: DAI is shared [ 2.575371] [ 2.575371] [McASP1][mcasp->base][FA460000] [ 2.581105] [ 2.581105] [McASP]not return [ 2.581105] [ 2.587643] davinci-mcasp 48464000.mcasp: DAI is shared [ 2.592907] [ 2.592907] [McASP2][mcasp->base][FA464000] [ 2.592907] [ 2.600090] [ 2.600090] [McASP]not return [ 2.600090] [ 2.606254] davinci-mcasp 48468000.mcasp: DAI is shared [ 2.611538] [ 2.611538] [McASP3][mcasp->base][FA468000] [ 2.611538] [ 2.618716] [ 2.618716] [McASP]not return [ 2.618716] [ 2.626218] NET: Registered protocol family 10 [ 2.641469] sit: IPv6 over IPv4 tunneling driver [ 2.646645] NET: Registered protocol family 17 [ 2.651160] can: controller area network core (rev 20120528 abi 9) [ 2.657433] NET: Registered protocol family 29 [ 2.661910] can: raw protocol (rev 20120528) [ 2.666399] Key type dns_resolver registered [ 2.670850] omap_voltage_late_init: Voltage driver support not added [ 2.677878] Power Management for TI OMAP4+ devices. [ 2.683023] Registering SWP/SWPB emulation handler [ 2.690578] dmm 4e000000.dmm: initialized all PAT entries [ 2.710492] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013). [ 2.717166] [drm] No driver support for vblank timestamp query. [ 2.734375] [drm] Enabling DMM ywrap scrolling [ 2.745940] mmc0: host does not support reading read-only switch, assuming write-enable [ 2.747925] @SD max clock = 10000000@ [ 2.748010] mmc0: new high speed SDHC card at address 59b4 [ 2.758505] mmcblk0: mmc0:59b4 SD 14.7 GiB [ 2.760268] mmcblk0: p1 p2 [ 2.787297] Console: switching to colour frame buffer device 160x50 [ 2.802966] mmc1: MAN_BKOPS_EN bit is not set [ 2.812173] @eMMC max clock = 25000000@ [ 2.819468] mmc1: new MMC card at address 0001 [ 2.830004] mmcblk1: mmc1:0001 MMC04G 3.57 GiB [ 2.840269] mmcblk1boot0: mmc1:0001 MMC04G partition 1 8.00 MiB [ 2.848982] omapdrm omapdrm.0: fb0: omapdrm frame buffer device [ 2.850543] mmcblk1boot1: mmc1:0001 MMC04G partition 2 8.00 MiB [ 2.860932] mmcblk1: p1 p2 [ 2.890270] [drm] Initialized omapdrm 1.0.0 20110917 on minor 0 [ 2.907245] hctosys: unable to open rtc device (rtc0) [ 2.924411] aic_dvdd: disabling [ 2.927605] vmmcwl_fixed: disabling [ 2.931336] ldousb: disabling [ 2.934815] ALSA device list: [ 2.937852] No soundcards found. [ 4.083086] EXT4-fs (mmcblk0p2): recovery complete [ 4.091778] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null) [ 4.099962] VFS: Mounted root (ext4 filesystem) on device 179:2. [ 4.138827] devtmpfs: mounted [ 4.142020] Freeing unused kernel memory: 336K (c08fc000 - c0950000) [ 4.148425] This architecture does not have kernel memory protection. [ 4.956804] systemd[1]: System time before build time, advancing clock. [ 5.066603] random: systemd: uninitialized urandom read (16 bytes read, 23 bits of entropy available) [ 5.080446] random: systemd: uninitialized urandom read (16 bytes read, 23 bits of entropy available) [ 5.092140] systemd[1]: systemd 229 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT +GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN) [ 5.110663] systemd[1]: Detected architecture arm. Welcome to Arago 2016.12! [ 5.138510] systemd[1]: Set hostname to <dra7xx-evm>. [ 5.313308] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 24 bits of entropy available) [ 5.329424] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read, 24 bits of entropy available) [ 5.339892] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read, 25 bits of entropy available) [ 5.370354] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 25 bits of entropy available) [ 5.386293] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 25 bits of entropy available) [ 5.687845] random: systemd: uninitialized urandom read (16 bytes read, 29 bits of entropy available) [ 5.697383] random: systemd: uninitialized urandom read (16 bytes read, 29 bits of entropy available) [ 5.707353] random: systemd: uninitialized urandom read (16 bytes read, 29 bits of entropy available) [ 5.873480] systemd[1]: Configuration file /etc/systemd/system/multi-user.target.wants/MAN2020.service is marked executable. Please remove executable permission bits. Proceeding anyway. [ 5.890546] systemd[1]: Configuration file /etc/systemd/system/multi-user.target.wants/MAN2020.service is marked world-writable. Please remove world writability permission bits. Proceeding anyway. [ 5.912440] systemd[1]: gplv3-notice.service: Service lacks both ExecStart= and ExecStop= setting. Refusing. [ 6.044402] systemd[1]: gplv3-notice.service: Cannot add dependency job, ignoring: Unit gplv3-notice.service is not loaded properly: Invalid argument. [ 6.058516] systemd[1]: sysinit.target: Found ordering cycle on sysinit.target/start [ 6.066306] systemd[1]: sysinit.target: Found dependency on alignment.service/start [ 6.074089] systemd[1]: sysinit.target: Found dependency on basic.target/start [ 6.081391] systemd[1]: sysinit.target: Found dependency on sockets.target/start [ 6.088839] systemd[1]: sysinit.target: Found dependency on avahi-daemon.socket/start [ 6.096707] systemd[1]: sysinit.target: Found dependency on sysinit.target/start [ 6.104160] systemd[1]: sysinit.target: Breaking ordering cycle by deleting job alignment.service/start [ 6.113615] systemd[1]: alignment.service: Job alignment.service/start deleted to break ordering cycle starting with sysinit.target/start [ SKIP ] Ordering cycle found, skipping alignment.service [ 6.151102] systemd[1]: Created slice User and Session Slice. [ OK ] Created slice User and Session Slice. [ 6.177120] systemd[1]: Reached target Swap. [ OK ] Reached target Swap. [ 6.197304] systemd[1]: Listening on Network Service Netlink Socket. [ OK ] Listening on Network Service Netlink Socket. [ 6.290942] systemd[1]: Listening on udev Kernel Socket. [ OK ] Listening on udev Kernel Socket. [ 6.317229] systemd[1]: Listening on /dev/initctl Compatibility Named Pipe. [ OK ] Listening on /dev/initctl Compatibility Named Pipe. [ 6.347193] systemd[1]: Listening on udev Control Socket. [ OK ] Listening on udev Control Socket. [ 6.377167] systemd[1]: Listening on Syslog Socket. [ OK ] Listening on Syslog Socket. [ 6.397181] systemd[1]: Listening on Journal Socket. [ OK ] Listening on Journal Socket. [ 6.417791] systemd[1]: Created slice System Slice. [ OK ] Created slice System Slice. [ 6.487173] systemd[1]: Mounting POSIX Message Queue File System... Mounting POSIX Message Queue File System... [ 6.519458] systemd[1]: Starting Remount Root and Kernel File Systems... Starting Remount Root and Kernel File Systems... [ 6.549608] systemd[1]: Starting Setup Virtual Console... Starting Setup Virtual Console... [ 6.577412] systemd[1]: Started Forward Password Requests to Wall Directory Watch. [ 6.579671] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null) [ OK ] Started Forward Password Requests to Wall Directory Watch. [ 6.657422] systemd[1]: Starting Create list of required static device nodes for the current kernel... Starting Create list of required st... nodes for the current kernel... [ 6.687334] systemd[1]: Started Dispatch Password Requests to Console Directory Watch. [ OK ] Started Dispatch Password Requests to Console Directory Watch. [ 6.717103] systemd[1]: Reached target Paths. [ OK ] Reached target Paths. [ 6.737108] systemd[1]: Reached target Slices. [ OK ] Reached target Slices. [ 6.787173] systemd[1]: Mounting Temporary Directory... Mounting Temporary Directory... [ 6.824991] systemd[1]: Starting Load Kernel Modules... Starting Load Kernel Modules... [ 6.849661] systemd[1]: Mounting Debug File System... Mounting Debug File System... [ 6.877106] systemd[1]: Reached target Remote File Systems. [ OK ] Reached target Remote File Systems. [ 6.907217] systemd[1]: Listening on Journal Socket (/dev/log). [ OK ] Listening on Journal Socket (/dev/log). [ 6.967393] systemd[1]: Starting Journal Service... Starting Journal Service... [ 6.987943] systemd[1]: Created slice system-serial\x2dgetty.slice. [ OK ] Created slice system-serial\x2dgetty.slice. [ 7.024541] systemd[1]: Mounted Debug File System. [ OK ] Mounted Debug File System. [ 7.047172] systemd[1]: Mounted POSIX Message Queue File System. [ OK ] Mounted POSIX Message Queue File System. [ 7.077124] systemd[1]: Mounted Temporary Directory. [ OK ] Mounted Temporary Directory. [ 7.096054] systemd[1]: Started Remount Root and Kernel File Systems. [ OK ] Started Remount Root and Kernel File Systems. [ 7.128358] systemd[1]: Started Setup Virtual Console. [ OK ] Started Setup Virtual Console. [ 7.158252] systemd[1]: Started Create list of required static device nodes for the current kernel. [ OK ] Started Create list of required sta...ce nodes for the current kernel. [ 7.188044] systemd[1]: systemd-modules-load.service: Main process exited, code=exited, status=1/FAILURE [ 7.198892] systemd[1]: Failed to start Load Kernel Modules. [FAILED] Failed to start Load Kernel Modules. See 'systemctl status systemd-modules-load.service' for details. [ 7.237027] systemd[1]: systemd-modules-load.service: Unit entered failed state. [ 7.244470] systemd[1]: systemd-modules-load.service: Failed with result 'exit-code'. [ 7.253327] systemd[1]: Started Journal Service. [ OK ] Started Journal Service. Starting Apply Kernel Variables... Starting Create Static Device Nodes in /dev... Starting udev Coldplug all Devices... Starting Flush Journal to Persistent Storage... [ OK ] Started Apply Kernel Variables. [ OK ] Started Create Static Device Nodes in /dev. [ 8.086592] systemd-journald[130]: Received request to flush runtime journal from PID 1 Starting udev Kernel Device Manager... [ OK ] Reached target Local File Systems (Pre). Mounting /var/volatile... Mounting /media/ram... [ OK ] Mounted /var/volatile. [ OK ] Mounted /media/ram. [ OK ] Started Flush Journal to Persistent Storage. [ OK ] Started udev Kernel Device Manager. [ OK ] Started udev Coldplug all Devices. [ OK ] Reached target Local File Systems. [ 8.992380] omap_rng 48090000.rng: OMAP Random Number Generator ver. 20 Starting Create Volatile Files and Directories... Starting Load/Save Random Seed... [ 9.106726] omap-des 480a5000.des: OMAP DES hw accel rev: 2.2 [ 9.154894] alg: skcipher: setkey failed on test 5 for ecb-des-omap: flags=100 [ OK ] Found device /dev/ttyS3.[ 9.209480] alg: skcipher-ddst: setkey failed on test 5 for ecb-des-omap: flags=100 [ 9.221155] alg: skcipher-ddst: setkey failed on test 5 for ecb-des-omap: flags=100 [ OK ] Started Load/Save Random Seed. [ OK ] Started Create Volatile Files and Directories. [ 9.315046] omap_rtc 48838000.rtc: rtc core: registered 48838000.rtc as rtc0 Starting Network Time Synchronization... Starting Update UTMP about System Boot/Shutdown... [ OK ] Started Update UTMP about System Boot/Shutdown. [ 9.718532] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec [ 9.727538] omap-sham 4b101000.sham: hw accel on OMAP rev 4.3 [ OK ] Started Network Time Synchronization. [ OK ] Reached target System Time Synchronized. [ 9.805902] SCSI subsystem initialized Starting Synchronize System and HW clocks... [ OK ] Started Synchronize System and HW clocks. [ OK ] Reached target System Initialization. [ OK ] Listening on D-Bus System Message Bus Socket. [ OK ] Listening on RPCbind Server Activation Socket. [ OK ] Started Daily Cleanup of Temporary Directories. [ OK ] Reached target Timers. [ OK ] Listening on dropbear.socket. [ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket. [ OK ] Reached target Sockets. [ OK ] Reached target Basic System. [ OK ] Started System Logging Service. [ OK ] Started Start helloworld. [ OK ] Started D-Bus System Message Bus. [ 10.493543] omap-aes 4b500000.aes: OMAP AES hw accel rev: 3.3 [ 10.570047] omap-aes 4b700000.aes: OMAP AES hw accel rev: 3.3 [ 10.579706] ahci 4a140000.sata: SSS flag set, parallel bus scan disabled [ 10.594465] ahci 4a140000.sata: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode [INFO] VERSION: B0.0.0.0004[ 10.620591] ahci 4a140000.sata: flags: 64bit ncq sntf stag pm led clo only pmp pio slum part ccc apst [SYS ] paring option: token=3, option=(null) [INFO] R3 init, iface=/dev/ttyS7 [INFO] R2 init [INFO] watchdog init [INFO] CLIENT ready [ 10.667248] scsi host0: ahci [ 10.670562] ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a1410ff] port 0x100 irq 339 [ 10.718119] [drm] Initialized pvr 1.14.3699939 20110701 on minor 1 [ 11.046969] ata1: SATA link down (SStatus 0 SControl 300) [ 11.204663] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck. Starting Network Service... [ OK ] Started strongSwan IPsec IKEv1/IKEv2 daemon using ipsec.conf. Starting Telephony service... Starting Permit User Sessions... Starting hw-id.service... Starting Login Service... Starting Avahi mDNS/DNS-SD Stack... Starting uim-sysfs.service... [ OK ] Started Kernel Logging Service. [ OK ] Started Permit User Sessions. [ OK ] Started hw-id.service. [ 12.065940] net eth0: initializing cpsw version 1.15 (0) [ 12.085624] net eth0: initialized cpsw ale version 1.4 [ 12.091516] FAT-fs (mmcblk1p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck. [ 12.109759] net eth0: ALE Table size 1024 [ 12.115792] libphy: PHY not found [ 12.137325] EXT4-fs (mmcblk1p2): recovery complete [ 12.146336] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null) [ OK ] Started Network Service. [ 12.195952] net eth0: phy "" not found on slave 0, err -19 [ 12.305966] net eth0: phy found : id is : 0x221560 [ 12.340777] cpsw-phy-sel 4a002554.cpsw-phy-sel: RMII External clock is not supported [ 12.446567] Bluetooth: Core ver 2.21 [ 12.459668] NET: Registered protocol family 31 [ 12.498372] Bluetooth: HCI device and connection manager initialized [ 12.504784] Bluetooth: HCI socket layer initialized [ 12.556991] Bluetooth: L2CAP socket layer initialized [ 12.562120] Bluetooth: SCO socket layer initialized [ 12.569817] NET: Registered protocol family 15 [ 12.605481] @@USB2PHY_TERMINATION_CONTROL=0x220004 [ 12.833130] Initializing XFRM netlink socket [ 13.150525] @@USB2PHY_TERMINATION_CONTROL=0x220004 [ 13.782874] usbcore: registered new interface driver usbfs [ 13.804934] usbcore: registered new interface driver hub [ 13.827968] usbcore: registered new device driver usb [ 13.882276] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller [ 13.900972] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1 [ 13.930702] xhci-hcd xhci-hcd.0.auto: hcc params 0x0220f04c hci version 0x100 quirks 0x00210010 [ 13.957021] xhci-hcd xhci-hcd.0.auto: irq 434, io mem 0x48890000 [ 13.977631] hub 1-0:1.0: USB hub found [ 13.987192] hub 1-0:1.0: 1 port detected [ 13.997396] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller [ 14.002923] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2 [ 14.027049] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM. [ 14.048642] hub 2-0:1.0: USB hub found [ 14.052450] hub 2-0:1.0: 1 port detected [ 14.057091] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller [ 14.062627] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 3 [ 14.087335] xhci-hcd xhci-hcd.1.auto: hcc params 0x0220f04c hci version 0x100 quirks 0x00210010 [ 14.096131] xhci-hcd xhci-hcd.1.auto: irq 435, io mem 0x488d0000 [ 14.128273] hub 3-0:1.0: USB hub found [ 14.132440] hub 3-0:1.0: 1 port detected [ 14.147512] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller [ 14.153042] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 4 [ OK ] Started Avahi mDNS/DNS-SD Stack.[ 14.204177] usb usb4: We don't know the algorithms for LPM for this host, disabling LPM. [ OK ] Started Telephony service. [ OK ] Started Login Service. [ OK ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch. [ OK ] Reached target Network. Starting Network Name Resolution... Starting Lightning Fast Webserver With Light System Requirements...[ 14.269159] hub 4-0:1.0: USB hub found [ OK ] Started Serial Getty on ttyS3. [ OK ] Reached target Login Prompts.[ 14.276887] hub 4-0:1.0: 1 port detected [[032m OK ]Started uim-sysfs.service. [[032m OK ]Started Lightning Fast Webserver With Light Sstem Requirements. [ OK ] Started Network Name Resolution. Starting rc.pvr.service... [ 14.918173] PVR_K: UM DDK-(3699939) and KM DDK-(3699939) match. [ OK ] [ OK ] Started rc.pvr.service. Starting telnetd.service... Starting tiipclad-daemon.service... [ OK ] Started telnetd.service. [ OK ] Started tiipclad-daemon.service. Starting thttpd.service... [ OK ] Started thttpd.service. Starting rng-tools.service... [ OK ] Started rng-tools.service. [ 15.386683] random: nonblocking pool is initialized Starting gdbserverproxy.service... [ OK ] Started gdbserverproxy.service. Starting matrix-gui-2.0.service... [ OK ] Started matrix-gui-2.0.service. Starting thermal-zone-init.service... [ OK ] Started thermal-zone-init.service. [ OK ] Reached target Multi-User System. Starting Update UTMP about System Runlevel Changes... [ OK ] Started Update UTMP about System Runlevel Changes. _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project http://arago-project.org dra7xx-evm ttyS3 Arago 2016.12 dra7xx-evm ttyS3 dra7xx-evm login: root (automatic login) root@dra7xx-evm:~# root@dra7xx-evm:~# root@dra7xx-evm:~# ls /dev/video* /dev/video0 /dev/video1 /dev/video10 /dev/video11 root@dra7xx-evm:~# root@dra7xx-evm:~# root@dra7xx-evm:~# root@dra7xx-evm:~# root@dra7xx-evm:~# v4l2-ctl --list-device wbcap (platform:omapwb-cap): /dev/video11 omapwb-m2m (platform:omapwb-m2m): /dev/video10 vpe (platform:vpe): /dev/video0 root@dra7xx-evm:~#
Here is our dts file =>
/* * Copyright (C) 2016 Texas Instruments Incorporated - http://www.ti.com/ * * This program is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License version 2 as * published by the Free Software Foundation. */ //#include "dra7-evm.dts" #include "dra7-evm-lcd-lg.dts" / { memory { device_type = "memory"; reg = <0x0 0x80000000 0x0 0x80000000>; /* 2 GB */ //reg = <0x0 0x80000000 0x0 0xC0000000>; /* 3 GB */ }; leds { status = "disabled"; }; gpio_keys { status = "disabled"; }; jamr3_sound{ status = "disabled"; }; primary_sound{ status = "disabled"; }; }; &evm_3v3_sd { gpio = <>; }; &snd0 { status = "disabled"; }; &hdmi0 { status = "disabled"; }; &tpd12s015 { status = "disabled"; }; &pcf_lcd { status = "disabled"; }; &pcf_gpio_21 { status = "disabled"; }; &lcd_fpd { status = "disabled"; }; &extcon_usb1 { //fake gpio id-gpios = <&gpio3 24 GPIO_ACTIVE_HIGH>; }; &extcon_usb2 { //fake gpio id-gpios = <&gpio3 25 GPIO_ACTIVE_HIGH>; }; &usb1 { dr_mode = "host"; }; &tlv320aic3106 { status = "disabled"; }; &pcf_hdmi { status = "disabled"; }; &i2c_p3_exp { ov10633@37 { status = "disabled"; }; }; &tvp_5158 { status = "disabled"; }; &disp_ser { status = "disabled"; }; &pcie1_rc { status = "disabled"; }; &elm { status = "okay"; }; #if 1 &gpmc { status = "okay"; ranges = <0 0 0x08000000 0x01000000>; /* minimum GPMC partition = 16MB */ nand@0,0 { compatible = "ti,omap2-nand"; reg = <0 0 4>; /* device IO registers */ interrupt-parent = <&gpmc>; interrupts = <0 IRQ_TYPE_NONE>, /* fifoevent */ <1 IRQ_TYPE_NONE>; /* termcount */ rb-gpios = <&gpmc 0 GPIO_ACTIVE_HIGH>; /* gpmc_wait0 pin */ ti,nand-ecc-opt = "bch8"; ti,elm-id = <&elm>; nand-bus-width = <16>; gpmc,device-width = <2>; gpmc,sync-clk-ps = <0>; gpmc,cs-on-ns = <0>; gpmc,cs-rd-off-ns = <80>; gpmc,cs-wr-off-ns = <80>; gpmc,adv-on-ns = <0>; gpmc,adv-rd-off-ns = <60>; gpmc,adv-wr-off-ns = <60>; gpmc,we-on-ns = <10>; gpmc,we-off-ns = <50>; gpmc,oe-on-ns = <4>; gpmc,oe-off-ns = <40>; gpmc,access-ns = <40>; gpmc,wr-access-ns = <80>; gpmc,rd-cycle-ns = <80>; gpmc,wr-cycle-ns = <80>; gpmc,bus-turnaround-ns = <0>; gpmc,cycle2cycle-delay-ns = <0>; gpmc,clk-activation-ns = <0>; gpmc,wr-data-mux-bus-ns = <0>; /* MTD partition table */ /* All SPL-* partitions are sized to minimal length * which can be independently programmable. For * NAND flash this is equal to size of erase-block */ #address-cells = <1>; #size-cells = <1>; partition@0 { label = "NAND.device.0"; reg = <0x00000000 0x10000000>; /*256 MB*/ }; /* partition@0 { label = "NAND.SPL"; reg = <0x00000000 0x000020000>; }; partition@1 { label = "NAND.SPL.backup1"; reg = <0x00020000 0x00020000>; }; partition@2 { label = "NAND.SPL.backup2"; reg = <0x00040000 0x00020000>; }; partition@3 { label = "NAND.SPL.backup3"; reg = <0x00060000 0x00020000>; }; partition@4 { label = "NAND.u-boot-spl-os"; reg = <0x00080000 0x00040000>; }; partition@5 { label = "NAND.u-boot"; reg = <0x000c0000 0x00100000>; }; partition@6 { label = "NAND.u-boot-env"; reg = <0x001c0000 0x00020000>; }; partition@7 { label = "NAND.u-boot-env.backup1"; reg = <0x001e0000 0x00020000>; }; partition@8 { label = "NAND.kernel"; reg = <0x00200000 0x00800000>; }; partition@9 { label = "NAND.file-system"; reg = <0x00a00000 0x0f600000>; }; */ }; }; #endif &qspi { status = "okay"; spi-max-frequency = <76800000>; m25p80@0 { compatible = "s25fl256s1"; spi-max-frequency = <76800000>; reg = <0>; spi-tx-bus-width = <1>; spi-rx-bus-width = <4>; #address-cells = <1>; #size-cells = <1>; /* MTD partition table. * The ROM checks the first four physical blocks * for a valid file to boot and the flash here is * 64KiB block size. */ partition@0 { label = "QSPI.MLO"; reg = <0x00000000 0x000040000>; }; partition@1 { label = "QSPI.u-boot"; reg = <0x00040000 0x00100000>; }; partition@2 { label = "QSPI.DRA7-evm.dtb"; reg = <0x00140000 0x00080000>; }; partition@3 { label = "QSPI.u-boot-env"; reg = <0x001c0000 0x00010000>; }; partition@4 { label = "QSPI.u-boot-env.backup1"; reg = <0x001d0000 0x0010000>; }; partition@5 { label = "QSPI.uImage"; reg = <0x001e0000 0x0800000>; }; partition@6 { label = "QSPI.IPU-exe"; reg = <0x009e0000 0x01620000>; }; }; }; &mailbox5 { status = "disabled"; }; &mailbox6 { status = "disabled"; }; &mmu0_dsp1 { status = "disabled"; }; &mmu1_dsp1 { status = "disabled"; }; &mmu0_dsp2 { status = "disabled"; }; &mmu1_dsp2 { status = "disabled"; }; &mmu_ipu1 { status = "disabled"; }; &mmu_ipu2 { status = "disabled"; }; &ipu2 { status = "disabled"; }; &ipu1 { status = "disabled"; }; &dsp1 { status = "disabled"; }; &dsp2 { status = "disabled"; }; &dss { status = "okay"; ports { port { reg = <1>; }; }; }; &hdmi { status = "disabled"; }; &vip1 { status = "disabled"; }; &video_in { status = "disabled"; }; &reserved_mem { status = "disabled"; }; &pcf_jamr3_21 { status = "disabled"; }; &tlv320aic3106a { status = "disabled"; }; &tlv320aic3106b { status = "disabled"; }; &tlv320aic3106c { status = "disabled"; }; &mcasp7 { status = "disabled"; }; &mcasp8 { status = "disabled"; }; &mcasp2 { status = "okay"; }; &mcasp3 { status = "okay"; }; &mcasp6 { status = "disabled"; }; &ipu2_cma_pool { status = "disabled"; }; &dsp1_cma_pool { status = "disabled"; }; &ipu1_cma_pool { status = "disabled"; }; &dsp2_cma_pool { status = "disabled"; }; &cmem_radio { status = "disabled"; }; &dsp1_sr0 { status = "disabled"; }; &uart4 { status = "okay"; }; &uart8 { status = "okay"; }; &uart5 { status = "okay"; }; &uart9 { status = "okay"; }; &uart10 { status = "okay"; }; &mmc4 { status = "disabled"; }; /*********************************below for video port enable test***************************************/ /* VIN2A pins mapped to VIP1 */ &vip2 { status = "okay"; //pinctrl-names = "default"; /* Pinmux conflict between vin1a:16-23 & vin2a:0-8 Either use full 24bit of vin1a or use 16bit vin1a and 8bitvin2a TO enable cam2, uncomment this pinctrl-0 = <&vin1a_pins &vin2a>; */ //pinctrl-0 = <&vin3a_pins >; }; &vin3a { status = "okay"; endpoint@0 { slave-mode; remote-endpoint = <&hdmi_receiver>; }; }; &i2c1 { status = "okay"; clock-frequency = <400000>; adv7611: adv7611@4c { compatible = "adi,adv7611"; reg = <0x4c>; port { hdmi_receiver: endpoint { remote-endpoint = <&vin3a>; hsync-active = <1>; vsync-active = <1>; pclk-sample = <1>; }; }; }; }; /**********************************up for video port enable test*****************************************/ &i2c1 { status = "okay"; clock-frequency = <400000>; }; &i2c2 { status = "okay"; clock-frequency = <400000>; }; &i2c3 { status = "okay"; clock-frequency = <400000>; }; &i2c4 { status = "okay"; clock-frequency = <400000>; }; &i2c5 { status = "okay"; clock-frequency = <400000>; }; &mcspi1 { status = "okay"; spidev@0 { spi-max-frequency = <24000000>; reg = <0>; compatible = "rohm,dh2228fv"; /*compatible = "linux,spidev";*/ }; }; &mcspi2 { status = "okay"; spidev@1 { spi-max-frequency = <24000000>; reg = <0>; compatible = "rohm,dh2228fv"; }; }; &mcspi3 { status = "okay"; spidev@2 { spi-max-frequency = <24000000>; reg = <0>; compatible = "rohm,dh2228fv"; }; }; &mcspi4 { status = "okay"; spidev@3 { spi-max-frequency = <24000000>; reg = <0>; compatible = "rohm,dh2228fv"; }; }; &mcasp1 { #sound-dai-cells = <0>; assigned-clocks = <&mcasp1_ahclkx_mux>; assigned-clock-parents = <&atl_clkin1_ck>; status = "okay"; op-mode = <0>; // MCASP_IIS_MODE // tdm-slots = <2>; // 4 serializer // serial-dir = < // 0: INACTIVE, 1: TX, 2: RX // 0 0 1 2 >; tx-num-evt = <32>; rx-num-evt = <32>; }; &mcasp2 { #sound-dai-cells = <0>; assigned-clocks = <&mcasp2_ahclkx_mux>; assigned-clock-parents = <&atl_clkin1_ck>; status = "okay"; op-mode = <0>; // MCASP_IIS_MODE // tdm-slots = <2>; // 4 serializer // serial-dir = < // 0: INACTIVE, 1: TX, 2: RX // 0 0 1 2 >; tx-num-evt = <32>; rx-num-evt = <32>; }; &mcasp3 { #sound-dai-cells = <0>; assigned-clocks = <&mcasp3_ahclkx_mux>; assigned-clock-parents = <&atl_clkin1_ck>; status = "okay"; op-mode = <0>; // MCASP_IIS_MODE // tdm-slots = <2>; // 4 serializer // serial-dir = < // 0: INACTIVE, 1: TX, 2: RX // 0 0 1 2 >; tx-num-evt = <32>; rx-num-evt = <32>; }; &atl { assigned-clock-parents = <&sys_clkin1>, <&dpll_abe_m2_ck>; }; &mac { status = "okay"; active_slave = <1>; }; &davinci_mdio { status = "okay"; micrel_phy_config { #address-cells = <1>; #size-cells = <0>; micrel,led-mode = <1>; clock-names = "rmii-ref"; clocks = <&rmii_50M_clock>; }; rmii_50M_clock: rmii-ref{ #clock-cells = <0>; compatible ="fixed-clock"; clock-frequency = <50000000>; }; }; &cpsw_emac1 { phy_id = <&davinci_mdio>, <4>; phy-mode = "rmii"; status = "okay"; }; &phy_sel { rmii-clock-ext; }; &oppdm_mpu { status = "disabled"; }; &epwmss0 { status = "okay"; }; #if 0 &ehrpwm0 { status = "okay"; }; #endif &ecap0 { status = "okay"; }; &epwmss1 { status = "okay"; }; #if 0 &ehrpwm1 { status = "okay"; }; #endif &ecap1 { status = "okay"; }; &epwmss2 { status = "okay"; }; #if 0 &ehrpwm2 { status = "okay"; }; #endif &ecap2 { status = "okay"; }; &dra7_pmx_core { pinctrl-names = "default"; pinctrl-0 = <&man2020_pins>; man2020_pins: man2020_pins { pinctrl-single,pins = < 0x3B0 (MUX_MODE0 | PIN_INPUT_PULLUP) /* spi1_cs0.spi1_cs0 */ 0x3B4 (MUX_MODE0 | PIN_INPUT_PULLUP) /* spi1_cs1.spi1_cs1 */ 0x3A4 (MUX_MODE0 | PIN_INPUT_PULLDOWN) /* spi1_sclk.spi1_sclk */ 0x3AC (MUX_MODE0 | PIN_INPUT_PULLDOWN) /* spi1_d0.spi1_d0 */ 0x3A8 (MUX_MODE0 | PIN_INPUT_PULLDOWN) /* spi1_d1.spi1_d1 */ 0x3C8 (MUX_MODE0 | PIN_INPUT_PULLDOWN) /* spi2_d0.spi2_d0 */ 0x3C4 (MUX_MODE0 | PIN_INPUT_PULLDOWN) /* spi2_d1.spi2_d1 */ 0x3CC (MUX_MODE0 | PIN_INPUT_PULLUP) /* spi2_cs0.spi2_cs0 */ 0x3C0 (MUX_MODE0 | PIN_INPUT_PULLDOWN) /* spi2_sclk.spi2_sclk */ 0x264 (MUX_MODE7 | PIN_INPUT_PULLDOWN) /* rgmii0_txd0.spi4_cs0 */ 0x260 (MUX_MODE7 | PIN_INPUT_PULLDOWN) /* rgmii0_txd1.spi4_d0 */ 0x25C (MUX_MODE7 | PIN_INPUT_PULLDOWN) /* rgmii0_txd2.spi4_d1 */ 0x258 (MUX_MODE7 | PIN_INPUT_PULLDOWN) /* RGMII0_TXD3.spi4_sclk */ 0x40C (MUX_MODE0 | PIN_INPUT_PULLUP) /* i2c2_scl.i2c2_scl */ 0x408 (MUX_MODE0 | PIN_INPUT_PULLUP) /* i2c2_sda.i2c2_sda */ 0x378 (MUX_MODE2 | PIN_INPUT_PULLUP) /* gpio6_11.i2c3_scl */ 0x374 (MUX_MODE2 | PIN_INPUT_PULLUP) /* gpio6_10.i2c3_sda */ 0x2AC (MUX_MODE10 | PIN_INPUT_PULLUP) /* mcasp1_aclkr.i2c4_sda */ 0x2B0 (MUX_MODE10 | PIN_INPUT_PULLUP) /* mcasp1_fsr.i2c4_scl */ 0x2B4 (MUX_MODE10 | PIN_INPUT | SLEWCONTROL) /* mcasp1_axr0.i2c5_sda */ 0x2B8 (MUX_MODE10 | PIN_INPUT | SLEWCONTROL) /* mcasp1_axr1.i2c5_scl */ 0x314 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* mcasp2_axr4.gpio1_4 */ 0x3D4 (MUX_MODE14 | PIN_INPUT_PULLUP | SLEWCONTROL) /* dcan1_rx.gpio1_15 */ 0x06C (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* gpmc_a11.gpio2_1 */ 0x070 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* GPMC_A12.gpio2_2 */ 0x0C0 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* gpmc_clk.gpio2_22 */ 0x0D4 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* gpmc_ben1.gpio2_27 */ 0x31C (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* mcasp2_axr6.gpio2_29 */ 0x154 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* vin2a_clk0.gpio3_28 */ 0x2E8 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* mcasp1_axr13.gpio6_4 */ 0x288 (MUX_MODE0 | PIN_INPUT_PULLDOWN) /* gpio6_14.gpio6_14 */ 0x418 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* Wakeup0.gpio1_0 */ 0x41C (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* WAKEUP1.gpio1_1 */ 0x320 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* mcasp2_axr7.gpio1_5 */ 0x2E0 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* mcasp1_axr11.gpio4_17 */ 0x2E4 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* mcasp1_axr12.gpio4_18 */ 0x2CC (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* mcasp1_axr6.gpio5_8 */ 0x2D0 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* mcasp1_axr7.gpio5_9 */ 0x2D4 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* mcasp1_axr8.gpio5_10 */ 0x2D8 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* mcasp1_axr9.gpio5_11 */ 0x2DC (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* mcasp1_axr10.gpio5_12 */ 0x23C (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* mdio_mclk.gpio5_15 */ 0x240 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* mdio_d.gpio5_16 */ 0x24C (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* uart3_txd.gpio5_19 */ 0x274 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* rgmii0_rxd2.gpio5_29 */ 0x278 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* rgmii0_rxd1.gpio5_30 */ 0x27C (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* rgmii0_rxd0.gpio5_31 */ 0x2EC (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* mcasp1_axr14.gpio6_5 */ 0x2F0 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* mcasp1_axr15.gpio6_6 */ 0x318 (MUX_MODE14 | PIN_INPUT_PULLDOWN | MUX_VIRTUAL_MODE12) /* mcasp2_axr5.gpio6_7 */ 0x30C (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* mcasp2_axr2.gpio6_8 */ 0x284 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* usb2_drvvbus.gpio6_13 */ 0x28C (MUX_MODE0 | PIN_INPUT_PULLDOWN) /* gpio6_15.gpio6_15 */ 0x290 (MUX_MODE0 | PIN_INPUT_PULLDOWN) /* gpio6_16.gpio6_16 */ 0x298 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* xref_clk1.gpio6_18 */ 0x29C (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* xref_clk2.gpio6_19 */ 0x2A0 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* xref_clk3.gpio6_20 */ 0x3E8 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* uart1_ctsn.gpio7_24 */ 0x3EC (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* uart1_rtsn.gpio7_25 */ 0x3F0 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* uart2_rxd.gpio7_26 */ 0x3F4 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* uart2_txd.gpio7_27 */ 0x204 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* VOUT1_D10.gpio8_10 */ 0x1E4 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* VOUT1_D2.gpio8_2 */ 0x3E4 (MUX_MODE0 | PIN_INPUT_PULLUP | SLEWCONTROL) /* uart1_txd.uart1_txd */ 0x3E0 (MUX_MODE0 | PIN_INPUT_PULLUP | SLEWCONTROL) /* uart1_rxd.uart1_rxd */ 0x3F8 (MUX_MODE2 | PIN_INPUT_PULLUP) /* uart2_ctsn.uart3_rxd */ 0x3FC (MUX_MODE1 | PIN_INPUT_PULLUP) /* uart2_rtsn.uart3_txd */ 0x33C (MUX_MODE4 | PIN_INPUT_SLEW) /* mcasp4_axr0.uart4_rxd */ 0x340 (MUX_MODE4 | PIN_INPUT_SLEW) /* mcasp4_axr1.uart4_txd */ 0x32C (MUX_MODE4 | PIN_INPUT_PULLUP) /* mcasp3_axr0.uart5_rxd */ 0x330 (MUX_MODE4 | PIN_INPUT_PULLUP) /* mcasp3_axr1.uart5_txd */ 0x334 (MUX_MODE3 | PIN_INPUT_PULLUP) /* mcasp4_aclkx.uart8_rxd */ 0x338 (MUX_MODE3 | PIN_INPUT_PULLUP) /* mcasp4_fsx.uart8_txd */ 0x344 (MUX_MODE3 | PIN_INPUT_PULLUP) /* mcasp5_aclkx.uart9_rxd */ 0x348 (MUX_MODE3 | PIN_INPUT_PULLUP) /* mcasp5_fsx.uart9_txd */ 0x394 (MUX_MODE2 | PIN_INPUT_PULLUP) /* mmc3_dat4.uart10_rxd */ 0x398 (MUX_MODE2 | PIN_INPUT_PULLUP) /* MMC3_DAT5.uart10_txd */ 0x39C (MUX_MODE2 | PIN_INPUT_PULLUP) /* MMC3_DAT6.uart10_ctsn */ 0x3A0 (MUX_MODE2 | PIN_INPUT_PULLUP) /* MMC3_DAT7.uart10_rtsn */ 0x2BC (MUX_MODE0 | PIN_INPUT_SLEW) /* mcasp1_axr2.mcasp1_axr2 */ 0x2C0 (MUX_MODE0 | PIN_INPUT_SLEW) /* mcasp1_axr3.mcasp1_axr3 */ 0x2C4 (MUX_MODE0 | PIN_INPUT_SLEW) /* mcasp1_axr4.mcasp1_axr4 */ 0x2C8 (MUX_MODE0 | PIN_INPUT_SLEW) /* mcasp1_axr5.mcasp1_axr5 */ 0x2A4 (MUX_MODE0 | PIN_INPUT_PULLDOWN) /* mcasp1_aclkx.mcasp1_aclkx */ 0x2A8 (MUX_MODE0 | PIN_INPUT_SLEW) /* mcasp1_fsx.mcasp1_fsx */ 0x2F8 (MUX_MODE0 | PIN_INPUT_SLEW | MUX_VIRTUAL_MODE9) /* mcasp2_fsx.mcasp2_fsx */ 0x2F4 (MUX_MODE0 | PIN_INPUT_PULLDOWN | MUX_VIRTUAL_MODE9) /* mcasp2_aclkx.mcasp2_aclkx */ 0x304 (MUX_MODE0 | PIN_INPUT_PULLDOWN | MUX_VIRTUAL_MODE12) /* mcasp2_axr0.mcasp2_axr0 */ 0x308 (MUX_MODE0 | PIN_INPUT_PULLDOWN | MUX_VIRTUAL_MODE12) /* mcasp2_axr1.mcasp2_axr1 */ 0x310 (MUX_MODE1 | PIN_INPUT_SLEW | MUX_VIRTUAL_MODE9) /* mcasp2_axr3.mcasp3_axr3 */ 0x324 (MUX_MODE0 | PIN_INPUT_PULLDOWN) /* mcasp3_aclkx.mcasp3_aclkx */ 0x328 (MUX_MODE0 | PIN_INPUT_SLEW) /* mcasp3_fsx.mcasp3_fsx */ 0x158 MUX_MODE4 /* vin2a_de0.VOUT2_DE */ 0x1C4 MUX_MODE4 /* vin2a_d23.VOUT2_D0 */ 0x1C0 MUX_MODE4 /* VIN2A_D22.VOUT2_D1 */ 0x1BC MUX_MODE4 /* VIN2A_D21.vout2_d2 */ 0x1B8 MUX_MODE4 /* VIN2A_D20.vout2_d3 */ 0x1B4 MUX_MODE4 /* vin2a_d19.VOUT2_D4 */ 0x1B0 MUX_MODE4 /* VIN2A_D18.VOUT2_D5 */ 0x1AC MUX_MODE4 /* vin2a_d17.VOUT2_D6 */ 0x1A8 MUX_MODE4 /* VIN2A_D16.vout2_d7 */ 0x1A4 MUX_MODE4 /* VIN2A_D15.vout2_d8 */ 0x1A0 MUX_MODE4 /* VIN2A_D14.VOUT2_D9 */ 0x19C MUX_MODE4 /* vin2a_d13.VOUT2_D10 */ 0x198 MUX_MODE4 /* vin2a_d12.VOUT2_D11 */ 0x194 MUX_MODE4 /* VIN2A_D11.VOUT2_D12 */ 0x190 MUX_MODE4 /* VIN2A_D10.VOUT2_D13 */ 0x18C MUX_MODE4 /* vin2a_d9.VOUT2_D14 */ 0x188 MUX_MODE4 /* vin2a_d8.VOUT2_D15 */ 0x184 MUX_MODE4 /* VIN2A_D7.VOUT2_D16 */ 0x180 MUX_MODE4 /* VIN2A_D6.vout2_d17 */ 0x17C MUX_MODE4 /* vin2a_d5.VOUT2_D18 */ 0x178 MUX_MODE4 /* vin2a_d4.VOUT2_D19 */ 0x174 MUX_MODE4 /* VIN2A_D3.vout2_d20 */ 0x170 MUX_MODE4 /* VIN2A_D2.vout2_d21 */ 0x16C MUX_MODE4 /* vin2a_d1.VOUT2_D22 */ 0x168 MUX_MODE4 /* vin2a_d0.VOUT2_D23 */ 0x160 MUX_MODE4 /* VIN2A_HSYNC0.vout2_hsync */ 0x164 MUX_MODE4 /* vin2a_vsync0.VOUT2_VSYNC */ 0x15C MUX_MODE4 /* VIN2A_FLD0.VOUT2_CLK */ 0x000 MUX_MODE3 /* gpmc_ad0.VOUT3_D0 */ 0x004 MUX_MODE3 /* gpmc_ad1.VOUT3_D1 */ 0x008 MUX_MODE3 /* gpmc_ad2.VOUT3_D2 */ 0x00C MUX_MODE3 /* GPMC_AD3.vout3_d3 */ 0x010 MUX_MODE3 /* gpmc_ad4.VOUT3_D4 */ 0x014 MUX_MODE3 /* gpmc_ad5.VOUT3_D5 */ 0x018 MUX_MODE3 /* GPMC_AD6.vout3_d6 */ 0x01C MUX_MODE3 /* GPMC_AD7.vout3_d7 */ 0x020 MUX_MODE3 /* GPMC_AD8.vout3_d8 */ 0x024 MUX_MODE3 /* GPMC_AD9.vout3_d9 */ 0x028 MUX_MODE3 /* GPMC_AD10.vout3_d10 */ 0x02C MUX_MODE3 /* GPMC_AD11.vout3_d11 */ 0x030 MUX_MODE3 /* gpmc_ad12.VOUT3_D12 */ 0x034 MUX_MODE3 /* gpmc_ad13.VOUT3_D13 */ 0x038 MUX_MODE3 /* gpmc_ad14.VOUT3_D14 */ 0x03C MUX_MODE3 /* gpmc_ad15.vout3_d15 */ 0x050 MUX_MODE3 /* GPMC_A4.VOUT3_D20 */ 0x054 MUX_MODE3 /* GPMC_A5.VOUT3_D21 */ 0x044 MUX_MODE3 /* GPMC_A1.VOUT3_D17 */ 0x048 MUX_MODE3 /* gpmc_a2.VOUT3_D18 */ 0x04C MUX_MODE3 /* GPMC_A3.vout3_d19 */ 0x040 MUX_MODE3 /* GPMC_A0.VOUT3_D16 */ 0x058 MUX_MODE3 /* GPMC_A6.VOUT3_D22 */ 0x05C MUX_MODE3 /* GPMC_A7.VOUT3_D23 */ 0x060 MUX_MODE3 /* GPMC_A7.VOUT3_HSYNC */ 0x064 MUX_MODE3 /* GPMC_A9.vout3_vsync */ 0x0BC MUX_MODE3 /* GPMC_CS3.vout3_clk */ 0x21C MUX_MODE4 /* VOUT1_D16.VIN3A_D0 */ 0x228 MUX_MODE4 /* VOU1_D19.VIN3A_D3 */ 0x238 MUX_MODE4 /* VOU1_D23.VIN3A_D7 */ 0x220 MUX_MODE4 /* VOU1_D17.VIN3A_D1 */ 0x22C MUX_MODE4 /* VOU1_D20.VIN3A_D4 */ 0x224 MUX_MODE4 /* VOU1_D18.VIN3A_D2 */ 0x230 MUX_MODE4 /* VOU1_D21.VIN3A_D5 */ 0x234 MUX_MODE4 /* VOU1_D22.VIN3A_D6 */ 0x1D0 MUX_MODE4 /* vout1_fld.VIN3A_CLK0 */ 0x36C MUX_MODE0 /* MMC1_SDCD.MMC1_SDCD */ 0x370 MUX_MODE0 /* MMC1_SDWP.MMC1_SDWP */ 0x254 (MUX_MODE2 | PIN_INPUT ) /* rgmii0_txctl.rmii1_rxd0 */ 0x250 (MUX_MODE2 | PIN_INPUT ) /* rgmii0_txc.rmii1_rxd1 */ 0x270 (MUX_MODE2 | PIN_OUTPUT ) /* rgmii0_rxd3.rmii1_txd0 */ 0x26C (MUX_MODE2 | PIN_OUTPUT ) /* rgmii0_rxctl.rmii1_txd1 */ 0x248 (MUX_MODE2 | PIN_INPUT ) /* uart3_rxd.rmii1_crs */ 0x268 (MUX_MODE2 | PIN_OUTPUT ) /* rgmii0_rxc.rmii1_txen */ 0x244 (MUX_MODE0 | PIN_INPUT ) /* RMII_MHZ_50_CLK.RMII_MHZ_50_CLK */ 0x3B8 (MUX_MODE5 | PIN_INPUT_PULLDOWN) /* spi1_cs2.MDIO_MCLK */ 0x3BC (MUX_MODE5 | PIN_INPUT_PULLDOWN) /* spi1_cs3.MDIO_D */ 0x434 MUX_MODE0 /* TDI.TDI */ 0x444 MUX_MODE0 /* RTCK.RTCK */ 0x448 MUX_MODE0 /* EMU0.EMU0 */ 0x44C MUX_MODE0 /* EMU1.EMU1 */ 0x294 (MUX_MODE9 | PIN_INPUT) /* xref_clk0.clkout2 */ 0x280 MUX_MODE0 /* usb1_drvvbus.usb1_drvvbus */ 0x000 MUX_MODE0 /* gpmc_ad0 */ 0x004 MUX_MODE0 /* gpmc_ad1 */ 0x008 MUX_MODE0 /* gpmc_ad2 */ 0x00C MUX_MODE0 /* GPMC_AD3.gpmc_ad3 */ 0x010 MUX_MODE0 /* gpmc_ad4 */ 0x014 MUX_MODE0 /* gpmc_ad5 */ 0x018 MUX_MODE0 /* GPMC_AD6.gpmc_ad6 */ 0x01C MUX_MODE0 /* GPMC_AD7.gpmc_ad7 */ 0x020 MUX_MODE0 /* GPMC_AD8.gpmc_ad8 */ 0x024 MUX_MODE0 /* GPMC_AD9.gpmc_ad9 */ 0x028 MUX_MODE0 /* GPMC_AD10.gpmc_ad10 */ 0x02C MUX_MODE0 /* GPMC_AD11.gpmc_ad11 */ 0x030 MUX_MODE0 /* gpmc_ad12 */ 0x034 MUX_MODE0 /* gpmc_ad13 */ 0x038 MUX_MODE0 /* gpmc_ad14 */ 0x03C MUX_MODE0 /* gpmc_ad15 */ 0x0B4 (MUX_MODE0 | PIN_OUTPUT) /* gpmc_cs0.gpmc_cs0 */ 0x0C4 (MUX_MODE0 | PIN_OUTPUT) /* gpmc_advn_ale.gpmc_advn_ale */ 0x0C8 (MUX_MODE0 | PIN_OUTPUT) /* gpmc_oen_ren.gpmc_oen_ren */ 0x0CC (MUX_MODE0 | PIN_OUTPUT) /* gpmc_wen.gpmc_wen */ 0x0D0 (MUX_MODE0 | PIN_OUTPUT) /* gpmc_ben0.gpmc_ben0 */ 0x0D8 (MUX_MODE0 | PIN_INPUT | SLEWCONTROL) /* gpmc_wait0.gpmc_wait0 */ >; }; mmc3_pins_default: pinmux_mmc3_default_pins { pinctrl-single,pins = < 0x380 (MUX_MODE0 | PIN_INPUT_PULLUP) /* MMC3_CMD.MMC3_CMD */ 0x37C (MUX_MODE0 | PIN_INPUT_PULLUP) /* mmc3_clk.mmc3_clk */ 0x384 (MUX_MODE0 | PIN_INPUT_PULLUP) /* mmc3_dat0.mmc3_dat0 */ 0x388 (MUX_MODE0 | PIN_INPUT_PULLUP) /* mmc3_dat1.mmc3_dat1 */ 0x38C (MUX_MODE0 | PIN_INPUT_PULLUP) /* mmc3_dat2.mmc3_dat2 */ 0x390 (MUX_MODE0 | PIN_INPUT_PULLUP) /* mmc3_dat3.mmc3_dat3 */ >; }; vin3a_pins: pinmux_vin3a_pins { pinctrl-single,pins = < 0x21C MUX_MODE4 /* VOUT1_D16.VIN3A_D0 */ 0x228 MUX_MODE4 /* VOU1_D19.VIN3A_D3 */ 0x238 MUX_MODE4 /* VOU1_D23.VIN3A_D7 */ 0x220 MUX_MODE4 /* VOU1_D17.VIN3A_D1 */ 0x22C MUX_MODE4 /* VOU1_D20.VIN3A_D4 */ 0x224 MUX_MODE4 /* VOU1_D18.VIN3A_D2 */ 0x230 MUX_MODE4 /* VOU1_D21.VIN3A_D5 */ 0x234 MUX_MODE4 /* VOU1_D22.VIN3A_D6 */ 0x1D0 MUX_MODE4 /* vout1_fld.VIN3A_CLK0 */ >; }; }; &pbias_mmc_reg { regulator-max-microvolt = <3300000>; }; &mmc3 { /* from mmc-1 */ status = "okay"; vmmc-supply = <&evm_3v3_sw>; bus-width = <4>; ti,non-removable; /* * SDCD signal is not being used here - using the fact that GPIO mode * is always hardwired. */ //cd-gpios = <&gpio7 12 GPIO_ACTIVE_LOW>; max-frequency = <64000000>; pinctrl-names = "default"; pinctrl-0 = <&mmc3_pins_default>; }; &lcd { enable-gpios = <>; /* P15, CON_LCD_PWR_DN */ };
Regards,
Shawn