This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

How to use three video inputs through ethernet connection TCP/IP.

How to use three video inputs through ethernet connection TCP/IP.I with NullSource it is only for single core or can i use NullSource for multiple cores.

  • Hi Munesha,

    I've forwarded this to the experts. Their feedback should be posted here.

    BR
    Tsvetolin Shulev
  • In reply to Cvetolin Shulev-XID:

    Hi,

    Can you clarify which TI device, SW for this question? You run RTOS or Linux?

    Regards, Eric
  • In reply to lding:

    VISION SDK 2.12 with TDA2XX and I run in Windows 7.

  • In reply to MUNESHA G:

    Hi Munesha,

    I have forwarded your question to an Ethernet expert.

    Regards,
    Yordan
  • Hello Munesha,

    I am assuming you want to use PC to send video streams.

    For receiving video inputs you can use null source link no. of channels set to 3. The VSDK has example use-case with TCP/IP on Null source link. You can refer to it @vision_sdk\examples\tda2xx\src\usecases\network_rx_tx\chains_networkRxDecDisplay.c

    • This use-case is configured for single channel receive only. You need to make below modifications to receive 3 channels.

    1. In current configuration done through NullSrcLink_CreateParams_Init() function (called from use-case), no. of channels is set to 1 (pPrm->outQueInfo.numCh = NULL_SRC_LINK_NUM_CHANNELS_DEFAULT)
    2. You need to override this in your use-case. Change below in file chains_networkRxDecDisplay.c

    ChainsCommon_SetNetworkRxPrms(

               &pUcObj->NullSourcePrm,

               &pUcObj->DecodePrm,

               pObj->captureOutWidth,

               pObj->captureOutHeight,

               1, <--change this to 3

               30

           );

    • You can use network_tx tools present in network_tools for sending streams from PC.

    Let me know if any issues.

    Regards,

    Prasad Jondhale
    Sr. Software Engineer, Automotive Processors, TI India

  • In reply to Prasad Jondhale:

    Thanks prasad,

    I made changes what you explained above .But i am able to access only one video i.e first channel it is not taking other two videos please suggest me.What other changes i have to do in both algplugin and usecase to access three videos.
  • In reply to MUNESHA G:

    Hello MUNESHA,

    Sorry for late reply, was on vacation last week.

    What command are you using on PC? Are you inputting three video files?

    Please share output of "p"(statistics) once you run this use-case.

    Regards,

    Prasad Jondhale
    Sr. Software Engineer, Automotive Processors, TI India

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.