This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TDA2EVM5777: Vision SDK Related queries

Part Number: TDA2EVM5777

Hi,

The Vision SDK version we are using is - 02_12_00

Our development board is Jacinto 6 

Following are the queries

1.       Why Vision SDK is NOT supporting the LCD interface?
2.       What we need to do to enable the LCD interface in vision SDK?
3.       Whether we will be able to integrate Processor SDK and Vision SDK binaries?
4.       From Where we can see the individual core binaries from the File system in vision SDK?
5.       In vision SDK DSS is configured from which M4 core? IPU 1 or IPU 2?
  • Hi Ganesh,

    I have forwarded your question to a VisionSDK expert.

    Regards,
    Yordan
  • In reply to Yordan Kamenov:

    Hi

    here is my comments

    1.       Why Vision SDK is NOT supporting the LCD interface?

    [Shiju] VSDK Bios only mode support both HDMI and LCD, on VSDK Linux + bios (where a15 running Linux) we support only HDMI and this is due the dsiplay controll is moved to M4 side. TDA2x has onchip HDMI.

    2.       What we need to do to enable the LCD interface in vision SDK?

    [Shiju] this need to be analyzed

    3.       Whether we will be able to integrate Processor SDK and Vision SDK binaries?

    [Shiju] yes its is possible - InfoAdas does somethinhg similar. Also VSDK Linux uses the Processor SDK Linux Kernel, uboot, filesytem, SGX stack etc.

    4.       From Where we can see the individual core binaries from the File system in vision SDK?

    [Shiju] \VSDK\vision_sdk\hlos\linux\targetfs\lib\firmware

    5.       In vision SDK DSS is configured from which M4 core? IPU 1 or IPU 2?

    [Shiju] For VSDK Bios its from IPU1 and for VSDK linus its from IPU2

  • In reply to Shiju Sivasankaran:

    Hi Shiju,

    To your reply in point 3 i have one question.

    Say if am running a QT application to show vehicle cluster dials in processsor SDK and i want to show camera feed in middle of User Interface after doing some processing (3d Surround View). So in order to accomplish this how we should use Processor SDK and Vision SDK.
  • In reply to Ganesh H:

    hi
    yes, it is possible, we do have an InfoADAS demo integarting SRV and cluster
    regards, Shiju
  • In reply to Shiju Sivasankaran:

    Hi Shiju,

    Is this example available with Vision SDK usecases . I didn't see this example along with samples.
  • In reply to Ganesh H:

    No, this UC is not part of VSDK. its an infoADAS demo, not yet relased externally

    regards, Shiju

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.