RTOS: NDK sockets

Tool/software: TI-RTOS

Hello,

 I have set up a TCP server and enabled  the socket’s options:  SO_RCVTIMEO , SO_SNDTIMEO.

I called recv() with the flag MSG_WAITALL  and I noticed that there is no timeout on recv() (i.e. after the time defined with SO_RCVTIMEO recv() still blocks())

From what I read I could not find an explicit answer but it sounded like that the timeout option should be in effect, if set ,even with MSG_WAITALL in recv().

I also tried removing the MSG_WAITALL from recv() (setting flags parameter to 0) and still recv() blocks forever without any timeout.

Can you please explain (or help fix)  why the timeout does not hold ?

Thanks 

Guy