How to use three video inputs through ethernet connection TCP/IP.I with NullSource it is only for single core or can i use NullSource for multiple cores.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Munesha,
I am assuming you want to use PC to send video streams.
For receiving video inputs you can use null source link no. of channels set to 3. The VSDK has example use-case with TCP/IP on Null source link. You can refer to it @vision_sdk\examples\tda2xx\src\usecases\network_rx_tx\chains_networkRxDecDisplay.c
ChainsCommon_SetNetworkRxPrms(
&pUcObj->NullSourcePrm,
&pUcObj->DecodePrm,
pObj->captureOutWidth,
pObj->captureOutHeight,
1, <--change this to 3
30
);
Let me know if any issues.
Hello MUNESHA,
Sorry for late reply, was on vacation last week.
What command are you using on PC? Are you inputting three video files?
Please share output of "p"(statistics) once you run this use-case.