Hi everyone,
I am trying to use a MultiCam usecase when there are less than 4 cams.
(Now, If I run the MultiCam usecase with 2 or 3 cams, there is nothing to be displayed.)
>> It is stuck in sync link, because 1 or 2 cams is not connected..
[CHAIN]
Capture(M4) > Sync(M4) > IPCOut_IPU1_0 -> IPCIn_A15 -> Display
Questions.
1. Please, give me any advice for this issue..
2. In capture link, there is a code like below.
/* new data frames have been captured, process them */
instId = (UInt32)Utils_msgGetPrm(pRunMsg);
Where the message(instId) comes from?
Best Regards,
Anderson