Part Number: TDA3
Tool/software: Starterware
Hello All,
I am following section 3.6 of VisionSDK_UserGuide_TDA3xx.pdf for QSPI_SD boot.
version of vision sdk is VISION_SDK_02_11_00_00.
I am using 15x15 TI TDA3xx EVM.
SW2 & SW3 Switch setting 10011000 10000001, SW8001 switch setting 0100 0001.
After performing steps 1, 2 & 3 from section 3.6.3 i get following output
[Cortex_M4_IPU1_C0] QSPI Flash writer application Enter Device type to use 1 - 1 bit read from flash 2 - 4 bit (Quad) read from flash $ > 2 MID - 1 DID - 18 Enter 0 for Erase-Only (without flashing any image) Note : File size should be less than 33554432 Bytes. Enter the file path to flash: C:\VISION_SDK_02_11_00_00\vision_sdk\build\scripts\qspi_sd_tda3xx-evm\sbl_qspi_sd Enter the Offset in bytes (HEX): 0x00 Erase Options: --------------- 0 -> Erase Only Required Region 1 -> Erase Whole Flash 2 -> Skip Erase Enter Erase Option: 1 Load Options: ------------- 0 -> fread using code (RTS Library) 1 -> load raw using CCS (Scripting console) Enter Load Option: 0 Reading 85048 bytes from file... Read 16384 bytes [19%] from file... Read 32768 bytes [38%] from file... Read 49152 bytes [57%] from file... Read 65536 bytes [77%] from file... Read 81920 bytes [96%] from file... Read 85048 bytes [100%] from file. Done!! QSPI whole chip erase in progress QSPI Erase completed QSPI file write started file size to write: 85048 Bytes
I followed following thread but it is not answered
https://e2eprivate.ti.com/tdax_adas_sw/f/309/p/6781/39118.aspx#39118
Regards,
Rahul