Tool/software: TI C/C++ Compiler
I am trying to execute surround view camera, i was using multicamera usecase,display shows only without camera view.so please suggest to get the output
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TI C/C++ Compiler
I am trying to execute surround view camera, i was using multicamera usecase,display shows only without camera view.so please suggest to get the output
Hi
are you using all 4 cameras of same type?
the moasic of 4 window output comes in the display only if a 4 cameras are working.
you can enter the sub-menu option
1: Change Display Channel (Support 4CH LVDS + Mosaic use-case only)
this will just display one camera at a time and see which all cameras are working in your set-up.
you can disconnect and reconnect the vision daughter card and de-seilizer boards, amke sure they are connected tightly
regards, Shiju
Hi
No code changes are required.
But make sure you have correct pin settings as per user guide. refer below section of VisionSDK_UserGuide_TDA2xx.pdf
2.3.2 Capture Pin Settings
regards, Shiju