I'm using Windows 7 x64, VisionSDK 2.10 and a TDA2xx board.
So far, I have successfully tested EDMA transfers using EDMA Low Level Driver which is dependent of SYS/BIOS (it uses a semaphore instance to be exact). I was using CCS and connected to the board via XDS debug probe.
However, I need to test the transfers in an existing VisionSDK usecase without SYS/BIOS dependence. I have found that there is a way using Chip Support Library. I refer to this document: http://www.ti.com/lit/ug/spru401j/spru401j.pdf . However I could not find "csl.h" and "csl_edma.h" anywhere that contain the functional API described in the above document (chapter 7-4). This wiki says where I can download the CSL for C6000: http://processors.wiki.ti.com/index.php/Chip_support_library. After downloading the package I still cannot find the API anywhere. I am overally confused about the CSL setup process. My code runs on the DSP C66x core.
I just need a guiding hand to help me setup a simple EDMA transfer correctly using the CSL for a usecase in VisionSDK.
I will appreciate any help.
Thank you.