Part Number: TDA3
Hi,
Can I estimate the power consumption for TDA3x during POR reset?
Regards,
Kenshow
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Roughly,
At running state:
Total consumption = Switching consumption + leakage currents
When SoC is at reset, can say almost no clocks are running and no switching consumption. therefore:
Total Consumption = leakage currents
Regards,
Stan
Hurdugaciu-san,
If I look into the TRM, I find that the device is broken into the following power domains (Section 3.4.1). These power domains are controlled through the POWERSTATE bit-field and I scanned the different domains for their default state. What I find is that the ISS, DSP{1 and 2} and EVE domains default to an ON state. Additionally, the Always ON domains will be in their ON state as well.
Bottom line: Some modules (VIP, IPU, DSS, and EFUSE) are disabled; most modules are powered with slow clocks.
Kevin
Power Domain | Default Power State |
PD_WKUPAON | |
PD_COREAON | |
PD_CAM | PM_CAM_PWRSTCTRL[1:0].POWERSTATE defaults to 0x00 (OFF) |
PD_IPU | PM_IPU_PWRSTCTRL[1:0].POWERSTATE defaults to 0x00 (OFF) |
PD_DSS | PM_DSS_PWRSTCTRL[1:0].POWERSTATE defaults to 0x00 (OFF) |
PD_CUSTEFUSE | PM_CUSTEFUSE_PWRSTCTRL[1:0].POWERSTATE defaults to 0x00 (OFF) |
PD_ISS | PM_ISS_PWRSTCTRL[1:0].POWERSTATE defaults to 0x03 (ON) |
PD_DSP1 | PM_DSP1_PWRSTCTRL[1:0].POWERSTATE defaults to 0x03 (ON) |
PD_DSP2 | PM_DSP2_PWRSTCTRL[1:0].POWERSTATE defaults to 0x03 (ON) |
PD_EVE | PM_EVE1_PWRSTCTRL[1:0].POWERSTATE defaults to 0x03 (ON) |
Hi,
AON = Always-ON
That is,
PD_COREAON
PD_WKUPAON and
PD_MMAON
Cannot be switch off.
Regards,
Stan