Hi
We are trying to flash the TDA3x EVM Reference board via UART. We dont have a JTAG for now.
Following the SBL_Userguide and Using the MFlash tool, we are facing the following issue.
We could send the initial sbl_mflash over the uart but after this stage the tool cannot proceed further and flash the QSPI images as expected.
We tried with the prebuilt binaries from SDK and our compiled binary images from Vision SDK 3.0. But cannot proceed further.
Attached the mflash logs,
Kindly help on this urgently.
Logs:
C:\Users\prsc\Desktop\Mflash>mflash_run_config.bat
C:\Users\prsc\Desktop\Mflash>SET sbl_mflash="sbl_mflash"
C:\Users\prsc\Desktop\Mflash>SET appimage_location="AppImage_BE"
C:\Users\prsc\Desktop\Mflash>SET appimage_offset="0x80000"
C:\Users\prsc\Desktop\Mflash>SET sbl_location="sbl"
C:\Users\prsc\Desktop\Mflash>SET sbl_offset="0x00"
C:\Users\prsc\Desktop\Mflash>SET uart_port_number="5"
C:\Users\prsc\Desktop\Mflash>ECHO 14:14:58.93
14:14:58.93
C:\Users\prsc\Desktop\Mflash>mflash -M "sbl_mflash" -P "5" -F "AppImage_BE" "0x8
0000" -F "sbl" "0x00"
Usage: mflash -M <sbl_mflash> -P <Port Number> -C [optional: to clean the QSPI F
lash]-F <fileName> <offset> -F <fileName> <offset> ... [PC] sbl_mflash sbl_mflas
h
[PC] File 0 AppImage_BE
[PC] Offset 0 0x80000
[PC] File 1 sbl
[PC] Offset 1 0x00
[PC] com \\.\COM5
[PC] ##########Starting USB/UART Flasing Utility##############
[PC] Put UART Boot Mode, make fresh UART connection & restart
[PC] Press Enter when done...
Baud = 115200
Parity = 2
StopBits = 0
ByteSize = 8[PC] Opening serial port successful
[RBL]0 [RBL]0 [RBL]0 [RBL]e0 [RBL]4 [RBL]1 [RBL]5 [RBL]1 [RBL]41 [RBL]4c
[RBL]7 [RBL]1 [RBL]13 [RBL]2 [RBL]1 [RBL]0 [RBL]12 [RBL]15 [RBL]1 [RBL]0
[RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0
[RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]14
[RBL]21 [RBL]1 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0
[RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0
[RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0
[PC] Requesting the ASIC ID
[RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]4 [RBL]1 [RBL]5 [RBL]1 [RBL]41 [RBL]4c
[RBL]7 [RBL]1 [RBL]13 [RBL]2 [RBL]1 [RBL]0 [RBL]12 [RBL]15 [RBL]1 [RBL]0
[RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0
[RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]14
[RBL]21 [RBL]1 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0
[RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0
[RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0 [RBL]0
[PC] Requesting PERI_REQ mode
[PC] Sending SBL_MFLASH filesize.
[PC] Size of sbl_mflash = 104626
[PC] Sending SBL_MFLASH... Please wait
[PC] File Size = 104626
[PC] ##
[PC] Transfer Complete. Time = 10.000
[PC] Opening port for sbl_mflash.
Baud = 12000000
Parity = 0
StopBits = 0
ByteSize = 8
[PC] Opening serial port successful.
Regards
Naveen K