Hi
We cannot run the ISP use-cases for capturing from OV10640
Hardware used is TI TDA3x EVM with OV10640 TIDA-00421 + TIDA-01005 Hub
In the capture setting,
OV10640 Sensor for SV - IMI (TDA3x ONLY) is selected
The Serialisers are not getting detected here
[IPU1-0] 43.307936 s: Detected UB964 !!!
[IPU1-0] 43.308058 s: Switching to 800MHz Mode !!!
[IPU1-0] 43.319038 s:
[IPU1-0] 43.319313 s: i2cMdSubmitChan: i2c1 transfer to slave address 0x74 failed
[IPU1-0] 43.319404 s: src/bsp_deviceI2c.c @ Line 580:
[IPU1-0] 43.319526 s: I2C1: DEV 0x74: WR 0x03 = 0xc5 ... ERROR !!!
[IPU1-0] 43.319618 s: src/bsp_deviceI2c.c @ Line 602:
[IPU1-0] 43.319679 s: I2C1: Error timeout 1 ms!!!
[IPU1-0] 43.319770 s: src/bsputils_ub960.c @ Line 1133:
[IPU1-0] 43.319831 s: Could not configure UB913 Ser !!!
[IPU1-0] 43.322637 s:
[IPU1-0] 43.322912 s: i2cMdSubmitChan: i2c1 transfer to slave address 0x76 failed
[IPU1-0] 43.323064 s: src/bsp_deviceI2c.c @ Line 580:
[IPU1-0] 43.323156 s: I2C1: DEV 0x76: WR 0x03 = 0xc5 ... ERROR !!!
[IPU1-0] 43.323278 s: src/bsp_deviceI2c.c @ Line 602:
[IPU1-0] 43.323339 s: I2C1: Error timeout 1 ms!!!
[IPU1-0] 43.323430 s: src/bsputils_ub960.c @ Line 1133:
[IPU1-0] 43.323491 s: Could not configure UB913 Ser !!!
Is there any usecase supported to test the sensor setup (OV10640 + UB964) ( TIDA-00421 + TIDA-01005 )
Do anything needs to be changed to support these.
Also Found a similar issue for TDA3x RVP boards here
https://e2e.ti.com/support/arm/automotive_processors/f/1021/t/623776
Kindly help