Tool/software: Linux
Booting from nor flash which I did consists of the following steps:
1. First :
set the SW2+SW3+SW5 for SD boot:
2. SECOND:
I used SD boot to entry the boot environment, download the uboot.bin(from PROCESSOR_SDK_VISION_03_00_00_00/ti_components/os_tools/linux/u-boot/u-boot) to 0x0800 0000 via tftp.
POWER off the EVM.
3.THIRD:
set the SW2+SW3+SW5 for NOR(XIP) boot, and POWER on the EVM:
But the output of UART is nothing! Why?