Other Parts Discussed in Thread: SYSBIOS
Dear kind people of TI forum,
I am trying to run TFDTP on TDA2x(VISION_SDK_02_12_01_00).
When i run the "TDFTPRx link + Display", i keep getting the following error:
ERROR: PBM_alloc() failure...exiting!
PBMQ_free count = 10239
However, when i try to use Network RX/TX usecases -> 1.Network RX + Display -> 1. TFDTP, i can not get anything on my port. The board seems to be waiting for data...
Here is what i have done so far:
- set NDK_PROC_TO_USE = ipu1_1 in cfg.mk
- NSP_TFDTP_INCLUDE=yes in cfg.mk
- UC_tfdtprx_display=yes in uc_cfg.mk
- set NullSource (IPU1_1) -> Display_Video in chains_networkRxDisplay.txt
- #define TFDTP_TX_STREAMING_MODE 1 in network_tx_priv.h
- rebuilt the network tools
- used --usetfdtp in network tools
Is there a solution for this error?
Thank you in advance,
Stefan.