Tool/software: Linux
hello, when I using DCAN software Demo to receive a single periodic(100ms ) messages, the system halted.and I try adjust the periodic more than 300ms,sytem run normal.
Please help me,Thank you!
here are some trace:
[IPU1-1] 45.769078 s: DCAN MSG Received:Id[0x51D] , Length : [8], Data [0 .. 7]0x00, 0x00, 0x00, 0x00, 0x40, 0x00, 0x1F, 0xFF
[IPU1-1] 45.770084 s: Assertion @ Line: 365 in /media/qnxi/work/sil-ti-visionsdk/vision_sdk/examples/tda2xx/src/modules/dcan/utils_dcan.c: status == 0 : failed !!!
[IPU1-1] 45.770267 s:
[IPU1-1] 45.770328 s: ### XDC ASSERT - ERROR CALLBACK START ###
[IPU1-1] 45.770389 s:
[IPU1-1] 45.770511 s: assertion failure: A_badContext: bad calling context. See GateMutex API doc for details.
[IPU1-1] 45.770603 s:
[IPU1-1] 45.770633 s: ### XDC ASSERT - ERROR CALLBACK END ###