Hi:
I'm a fresh man in Vision SDK,I have installed the package of PROCESSOR_SDK_VISION_03_02_00_00 in Windows 10 OS , and then I build the package successfully with gmake tool;
I have read several documents in the Vision SDK , and I build the "vision_sdk_usecase_gen" successfully,even I generate a "vision_sdk_usecase_gen" project with Code Block , I add an empty algorithm in the
usecase gen tool ,and it can runs ok;
Now , I want to create a new usecase project with CodeBlock ,I follow the steps showed on page 7th in "VisionSDK_DevelopmentGuide.pdf" ,when I use the SourceCode in "C:\PROCESSOR_SDK_VISION_03_02_00_00\vision_sdk\apps\src\rtos\usecases\vip_single_cam_frame_copy" to
create a new project which include source code file such as "chains_vipSingleCameraFrameCopy.c"、"chains_vipSingleCameraFrameCopy_priv.c"、"chains_vipSingleCameraFrameCopy_priv.h" and a main.cpp with an empty main function;
When I build the new project , many problem arise ; for example , in the "system_linkId.h" , SYSTEM_MAKE_LINK_ID is not defined , it is an selective compile item in the file ; "UInt32" is not defined , I search it in the two included head files "stdint.h" and "system_procId.h" , I can't find the definition of "UInt32" !
many many problems !
How can I solve these problem; I can't find a project as example;