Hello,
how can I change easily the sensor type in the demonstration software? I'm using the RVP which has the OV10640 as video sensors. For our own development we have to use the OV10635 with exactly the same interface connection (MIPI CSI-2) and I2C via CSI2 to control the sensor.
I see, that the FVID2 supports the required OV10635 sensor and I also saw that this sensor is still used in the non ISS-usecases, but I'm not confident on how it is meant to tell the VSDK system using this sensor in the given ISS usecases.
In case of the OV10640 sensor I also saw, that there is a mode containing the letters "IMI" which seems having to do with the I2C interface. Is that the mode, which I need for stupid sensors, that require their setup by I2C commands send over MIPI CSI2? I'm a little bit confused about what I need.
Thanks a lot in advance for helping me!
Regards,
Guenter