Hi,
I want to generate the inData and inHeader for TIDL_OD by using my own video.
I use the same way as generating the segmentation use-case video.
My own file on the seg use-case works, but i will show the below error on the OD use-case.
[IPU1-0] 1301.978649 s: Assertion @ Line: 220 in nullSrcLink_tsk.c: frameLength < bitstreamBuf->bufSize : failed !!!
[IPU1-0] 1301.979167 s: Assertion @ Line: 220 in nullSrcLink_tsk.c: frameLength < bitstreamBuf->bufSize : failed !!!
[IPU1-1] 1301.923900 s: SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1023
[IPU1-1] 1301.924052 s: SYSTEM: Heap = LOCAL_DDR @ 0x00000000, Total size = 655360 B (640 KB), Free size = 643328 B (628 KB)
[HOST ] 1301.924388 s: SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1023
[HOST ] 1301.924418 s: SYSTEM: Heap = LOCAL_DDR @ 0x00000000, Total size = 6291456 B (6144 KB), Free size = 6224776 B (6078 KB)
Is there any difference between the input format of the two use-case?
Thank you in advance.
Best Regards,
Eric Lai