Tool/software: Linux
How to get the serial number of the chip of tda2x
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Please refer to Table 1-2. DIE_ID in the device TRM.
Although not explicitly stated, I think DIE_ID is a unique die ID identificator.
Regards,
Stan
Hi
Are you suggesting that you would like to use the chip ID as an input for the encryption process - is the encryption based on the chip id itself or a device unique key
Hi
Can you clarify where will you need to read the chip id from
If it is from user space, you have to resort to one of the following
1. Read from RTOS(on M4) , pass this information as part of IPC to application on A15
2. On A15 Use tool like omapconf and some scripting to pass this information to your application
3. Emulate ompaconf type mapping from a custom driver to map and read the device id information