Tool/software: TI C/C++ Compiler
Hello TI Applications Engineers,
I am currently developing on the TDA2PXEVM with fusion application board using the vision SDK, and attempting to interface with the DS90UB953EVM.
By loading the prebuilt binaries for version 3.04 of the SDK onto an SD card, I can reach the demo usecases menu via serial terminal. However, when I try to run Single Camera Usecases -> 1 CH UIP Capture + Display to talk to the image sensor on the DS90UB953EVM, I get the error "i2c4 transfer to slave address 0x30 failed". This is after setting up the DS90UB953EVM according to its user guide.
I tried modifying the slave ID and slave ID alias registers on the DS90UB953EVM via Analog Launchpad, but that didn't seem to help. My thought was that the deserializer i2c addressing registers on the fusion application board need to be configured to match those of the serializer on the DS90UB953EVM.
I attempted to gain access to these registers by loading version 3.03 of the SDK (version 3.04 failed to compile, I kept getting "system cannot find file specified" errors) from CCS (version 8.1.0) rather than booting from SD card. Following the user guide, I was able to load all the specified binaries onto their respective cores, except for "vision_sdk_a15_0_debug.xa15fg", which is supposed to go on CortexA15_0, but doesn't show up when I search for it in windows explorer.
Any help with these issues would be greatly appreciated.
Thanks,
Richard