Tool/software: Linux
Dear Sir:
We are using VSDK 03_04_00_00.
We try to use the CSI2 format to capture from the MIPI interface. When setting the inCsi2DataFormat to SYSTEM_CSI2_YUV422_8B, it is okay. However when trying using the SYSTEM_CSI2_YUV420_8B or SYSTEM_CSI2_YUV420_8B_LEGACY, it fail to create the ISSCAPTURE link. By tracing the code, I see that the underlying link only support SYSTEM_CSI2_YUV422_8B, but not supporting the 420 format. But if tracing the PDK driver, we can see there is no such forbidden case in the PDK.
Because the heat problem in the CPU, we want to try lower down the CSI2 transmitted data to reduce the heat when 8 channel(4CH in Parallel and 4 CH in CSI-2) are using in our board.
My question is that: is it possible to use YUV420_8B or 420_8B_LEGACY in the PDK? Because both of these 2 types sending less data through the CSI-2 interface. Dos PDK support it? Or does TI has any plan to support it in ISSCAPTURE link in the future?
Regards,
/ckhsu