This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
James,
Can you please also explain the connectivity of the following pins on the TPS65910A:
1. SCL_SCK
2. SDA_SDI
3. SDASR_EN2
4. SCLSR_EN1
The customer is not clear on the purpose and the usage of these connections.
Naveen M94353,
The board identification EEPROM is for TI's software to determine what board is the software running on. It enables correct loading of drivers as not all peripherals are used in all the boards where the SDK software might be loaded.
Thanks.