Hello,
We have few AM335x DDR3 Questions from our 3P.
We understood that the Datasheet's "DDR3 Routing Guidelines" should
be strictly followed, but we wonder if the below kind of usage leads to a problem.
AM3352 High-Speed Bypass Capacitors:
- Datasheet Table 5-56 mentions VDDS_DDR HS bypass capacitor count as "20"
isn't this number a little bit more. There are only 7 VDDS_DDR pins.
so we have only one capacitor on each pin. Will this be a problem?
Longest Manhattan distance for the data bus:
- In the Datasheet DQLMn is defined as DQ Longest Manhattan distance.
Is it possible to let us know the reason behind choosing DQLMx as Longest Manhattan distance.
In our case instead of DQLMx = 37mm, in order to maintain Length matching with all the address
signal group, DQLMx will be 45mm. Will this be a problem?
Trace spacing:
- "Center-to-center DQ[x] to other DDR3 trace spacing" is mentioned as 4W
but in our case that could be <4W(2W)
and also DQ[x] to other DQ[x] trace spacing is mentioned as 3W
but in our case that could be <3W(2W).
Will this lead to a problem?
Regards.