Dear All,
I am using am3517 controller with this controller i designed board with 18bit RGB display it is working fine in portrait mode but i need to rotate display for my application
following are the setting i had done. I am using TechNexion core module and their XUKR source.
1.In u-boot, add the following to the video_mode variable "omapfb.rotate=1 omapfb.vrfb=y"
2.Enabled "Framebuffer console rotation" in kernel configuration and compiled kernel with this setting enabled.
When i pass video mode variables in u-boot and without framebuffer console rotation is not set Display is showing up boot-up Image(penguine) which is rotated
and there is a cursor blinking but with video mode variables in u-boot and framebuffer console rotation =y, Then nothing gets displayed on screen not even Boot-up image
Following is the error on debug port
Starting Dropbear SSH server: dropbear.
[ 11.847076] detected analogics1 fb_set_par error, error code: -22
ioctl FBIOPUT_VSCREENINFO: Invalid argument
Starting PVR
[ 11.925415] pvrsrvkm: module is from the staging directory, the quality is unknown, you have been warned.
[ 11.989440] omaplfb: module is from the staging directory, the quality is unknown, you have been warned.
[ 12.021728] bufferclass_ti: module is from the staging directory, the quality is unknown, you have been warned.
Exiting, name server cannot be used: Temporary failure in name resolution (-3) 2 Jan 10:47:02 ntpdate[891]: name server cannot be used: Temporary failure in name res)
Starting GPE display manager: gpe-dm
.---O---.
| | .-. o o
| | |-----.-----.-----.| | .----..-----.-----.
| | | __ | ---'| '--.| .-'| | |
| | | | | |--- || --'| | | ' | | | |
'---'---'--'--'--. |-----''----''--' '-----'-'-'-'
-' |
'---'
The Angstrom Distribution devkit ttyO0
Angstrom v2011.06 devkit ttyO0
devkit login: Sending discover...
[ 14.434600] omapdss MANAGER error: dispc_setup_plane failed for ovl 0
[ 14.441375] omapdss MANAGER error: configure_overlay 0 failed
[ 14.545959] offset0 0, offset1 0, row_inc 3617, pix_inc 1
[ 14.556396] offset0 0, offset1 0, row_inc 3617, pix_inc 1
[ 14.873748] offset0 0, offset1 0, row_inc 3617, pix_inc 1
[ 14.892974] omapdss MANAGER error: dispc_setup_plane failed for ovl 0
[ 14.899749] omapdss MANAGER error: configure_overlay 0 failed
[ 14.984344] offset0 0, offset1 0, row_inc 3617, pix_inc 1
[ 14.990478] offset0 0, offset1 0, row_inc 3617, pix_inc 1
[ 15.016448] offset0 0, offset1 0, row_inc 3617, pix_inc 1
[ 15.301574] offset0 0, offset1 0, row_inc 3617, pix_inc 1
[ 15.320800] omapdss MANAGER error: dispc_setup_plane failed for ovl 0
[ 15.327575] omapdss MANAGER error: configure_overlay 0 failed
[ 15.414459] offset0 0, offset1 0, row_inc 3617, pix_inc 1
[ 15.423309] offset0 0, offset1 0, row_inc 3617, pix_inc 1
[ 15.441375] offset0 0, offset1 0, row_inc 3617, pix_inc 1
No lease, failing
any suggestions and
Thanks and Regards,
Rajeev .