• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » ARM® Processors » Sitara™ ARM® » AM3x Sitara ARM Processors Forum » i2c1 at u-boot level
Share
Sitara™ ARM®
  • Forum
  • Announcements
Options
  • Subscribe via RSS

i2c1 at u-boot level

i2c1 at u-boot level

This question is not answered
Keldy
Posted by Keldy
on Apr 11 2012 00:11 AM
Expert1780 points

Hi,

i want to use i2c1 at u-boot level. i'm using u-boot code from AM335x EVM, in u-boot code "board/ti/am335x/evm.c" i saw the include file <i2c.h>, and how it use to enable i2c0,

can i really use <i2c.h> header file to enable i2c1 as well? any changes needed?

Thanks

Keldy

sdk AM335x EVM AM335x PSP am335x_evm_config u-boot
Report Abuse
  • Reply
You have posted to a forum that requires a moderator to approve posts before they are publicly available.
All Replies
  • Anil
    Posted by Anil
    on Apr 11 2012 07:24 AM
    Expert6655 points

    Hi Keldy,

    In u-boot i2c0 is enabled by default, you can go through "read_eeprom()" API for usage.

    can i really use <i2c.h> header file to enable i2c1 as well? any changes needed?

    Yes, you have to add i2c.h

    i2c1 sould be register in the simillar lines as that of i2c0.

    * Do proper pinmuxing

    * enable i2c1 clocks

    * i2c_int()

    Note: In software I2C instances are starting from 1 instead of 0 (HW)

    Regards

    AnilKumar

    Please mark this Forum post as answered via the Verify Answer button below if it helps answer your question.  Thanks!

    AM335x PSP I2C
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Gururaja Hebbar
    Posted by Gururaja Hebbar
    on Apr 11 2012 22:58 PM
    Intellectual2535 points

    Also you need to setup pin-mux for i2c1 pins.

    so you need to setup

    1. i2c1 clocks

    2. i2c1 pin-mux

    3. proper i2c1 base address to be used by omap-i2c driver

    4. verify that the omap-i2c driver supports multi-bus and use it accordingly

    Regards

    Gururaja

    Does this help with your question? If not, please send back more information. If it answers your question, please click the  Verify Answer  button.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Keldy
    Posted by Keldy
    on Apr 12 2012 02:21 AM
    Expert1780 points

    Hi All,

    I build a i2c1 function inside u-boot code, ("board-support/u-boot-2011.09-psp04.06.00.02/board/ti/am335x/evm.c"), in this case, i plan to communicate with i2c port expander (tca6416) with chip address 0x20, communication speed 400k.

    ___________________________________________________________________

    void i2c1(void)
    {
     u32 val;
     val = __raw_readl(CONF_SPI0_D1);            //pin_mux i2c1_sda
     val = (val & 0xFFFFFFF1 | 0x2);
     __raw_writel(val, CONF_SPI0_D1);

     val = __raw_readl(CONF_SPI0_CS0);            //pin_mux i2c1_scl
     val = (val & 0xFFFFFFF1 | 0x2);
     __raw_writel(val, CONF_SPI0_CS0);

     i2c_init(400000, 0x20); //i2c speed 400k, i2c port expander (tca6416) chip address 0x20
     
     printf("sending value = 0xFF\n");           //write value
     i2c_write(0x20, 0x06, 1, 0xFF, 1);
     
     uchar read_val;        //read value
     printf("reading value :");
     i2c_read(0x20, 0x06, 1, &read_val, 1);
     printf("%d\n", read_val); 
    }

    ___________________________________________________________________

    am i correct? is the i2c_init(), i2c_write(), i2c_read() functions applicable for i2c1 ?

    Thanks & Regards

    Keldy  

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Gururaja Hebbar
    Posted by Gururaja Hebbar
    on Apr 12 2012 03:09 AM
    Intellectual2535 points

    I dont think thats enough. By default u-boot i2c driver will be working for i2c-0 instance. so you need to switch it to i2c-1 instance.

    Also look at board-support/u-boot-2011.09-psp04.06.00.02/board/ti/am335x/mux.c on how i2c0 pin-mux is done. 

    Have you set i2c1 clocks (controller clocks & not i2c device clocks). for this look at board-support/u-boot-2011.09-psp04.06.00.02/board/ti/am335x/pll.c

    Does this help with your question? If not, please send back more information. If it answers your question, please click the  Verify Answer  button.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Keldy
    Posted by Keldy
    on Apr 12 2012 03:42 AM
    Expert1780 points

    Hi,

    in "board-support/u-boot-2011.09-psp04.06.00.02/board/ti/am335x/mux.c"

    i have changed: PULLUDEN to PULLUDDIS (because i use external pull-up)

    static struct module_pin_mux i2c1_pin_mux[] = {
     {OFFSET(spi0_d1), (MODE(2) | RXACTIVE | PULLUDDIS | SLEWCTRL)}, /* I2C_DATA */
     {OFFSET(spi0_cs0), (MODE(2) | RXACTIVE | PULLUDDIS | SLEWCTRL)}, /* I2C_SCLK */
     {-1},
    };

    and i have add new function:

    void enable_i2c1_pin_mux(void)
    {
     configure_module_pin_mux(i2c1_pin_mux);
    }

    in "board-support/u-boot-2011.09-psp04.06.00.02/board/ti/am335x/evm.c"

    void i2c1(void)
    {

    enable_i2c1_pin_mux(); //set pin mux
     
     /* enable clock i2c1 */
     __raw_writel(0x2, CM_PER_I2C1_CLKCTRL);
     while (__raw_readl(CM_PER_I2C1_CLKCTRL) != 0x2);
     
     i2c_init(400000, 0x20); //i2c speed 400k, chip address 0x20
     
     printf("sending value = 0xFF\n");           //write value
     i2c_write(0x20, 0x06, 1, 0xFF, 1);
     
     uchar read_val;        //read value
     printf("reading value :");
     i2c_read(0x20, 0x06, 1, &read_val, 1);
     printf("%d\n", read_val); 
     
    }

    how i switch u-boot i2c driver to i2c-1 instance?

    Thanks & Regards

    Keldy

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Anil
    Posted by Anil
    on Apr 12 2012 12:33 PM
    Expert6655 points

    Hi Keldy,

    Replace this line
     i2c_init(400000, 0x20); //i2c speed 400k, chip address 0x20

    with
     i2c_init(400000, 2); //i2c speed 400k, chip id 2 /* instance 1 */

    Regards

    AnilKumar

    Please mark this Forum post as answered via the Verify Answer button below if it helps answer your question.  Thanks!

    AM335x PSP I2C
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Keldy
    Posted by Keldy
    on Apr 13 2012 05:28 AM
    Expert1780 points

    Hi,

    my u-boot hang while execute the i2c1() function, the i2c_write() cause the u-boot hang.

    void i2c1 (void)

    {

     enable_i2c1_pin_mux();
     
     /* enable clock i2c1 */
     __raw_writel(0x2, CM_PER_I2C1_CLKCTRL);
     while (__raw_readl(CM_PER_I2C1_CLKCTRL) != 0x2);
     
     i2c_init(400000, 2); //i2c speed 400k, chip address 0x20
     
     printf("sending value = 0xFF\n");           //write value
     i2c_write(0x20, 0x06, 1, 0xFF, 1);         //-----------------------------------------------------------------------------this line cause the u-boot hang
     uchar read_val;        //read value
     printf("reading value :");
     i2c_read(0x20, 0x06, 1, &read_val, 1);
     printf("%d\n", read_val); 
    }

    Any wrong with my code, what i have miss to configure?

    Thanks & Regards

    Keldy

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Prabhakar Lad
    Posted by Prabhakar Lad
    on Apr 13 2012 06:12 AM
    Genius4675 points

    Hi Keldy,

    Looking at the board/ti/am335x/evm.c , only  pinmuxing and i2c_init is done did you add both these in
    board_init() function itself? are you sure the i2c speed for i2c1 is 400000?

    Thx,

    --Prabhakar Lad

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Anil
    Posted by Anil
    on Apr 13 2012 06:21 AM
    Expert6655 points

    Hi Keldy,

    Remove "enable clock i2c1" code from your9 part. Because all the I2C clocks are enabled in u-boot in "pll_init()"

    You have to call your API (i2c1) after pll_init() call.

    Regards

    AnilKumar

    Please mark this Forum post as answered via the Verify Answer button below if it helps answer your question.  Thanks!

    AM335x PSP I2C
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Keldy
    Posted by Keldy
    on Apr 15 2012 21:15 PM
    Expert1780 points

    Hi,

    in "/board-support/u-boot-2011.09-psp04.06.00.02/board/ti/am335x/evm.c

    under function: s_init(void) :

    void s_init(void)
    {
     /* Can be removed as A8 comes up with L2 enabled */
     l2_cache_enable();

     /* WDT1 is already running when the bootloader gets control
      * Disable it to avoid "random" resets
      */
     __raw_writel(0xAAAA, WDT_WSPR);
     while(__raw_readl(WDT_WWPS) != 0x0);
     __raw_writel(0x5555, WDT_WSPR);
     while(__raw_readl(WDT_WWPS) != 0x0);

    #ifdef CONFIG_SPL_BUILD
     /* Setup the PLLs and the clocks for the peripherals */
     pll_init();
     i2c1();  ---------------------------------------------------------------- my API i2c1();

    The u-boot no hang anymore, but seen like the u-boot didn't execute i2c1(), because it didn't printf the message inside the i2c1(void) function.

    do i need to call the function s_init() inside board_init() function ?

    Thanks & Regard

    Keldy

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Anil
    Posted by Anil
    on Apr 16 2012 01:08 AM
    Expert6655 points

    Hi Keldy,

    Can you add next to config_am335x_ddr();? I think console is not initialized at your step.

    Regards

    AnilKumar

    Please mark this Forum post as answered via the Verify Answer button below if it helps answer your question.  Thanks!

    AM335x PSP I2C
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Keldy
    Posted by Keldy
    on Apr 16 2012 03:26 AM
    Expert1780 points

    Hi,

    void s_init(void)
    {
     /* Can be removed as A8 comes up with L2 enabled */
     l2_cache_enable();

     /* WDT1 is already running when the bootloader gets control
      * Disable it to avoid "random" resets
      */
     __raw_writel(0xAAAA, WDT_WSPR);
     while(__raw_readl(WDT_WWPS) != 0x0);
     __raw_writel(0x5555, WDT_WSPR);
     while(__raw_readl(WDT_WWPS) != 0x0);

    #ifdef CONFIG_SPL_BUILD
     /* Setup the PLLs and the clocks for the peripherals */
     pll_init();
     
     /* UART softreset */
     u32 regVal;
     u32 uart_base = DEFAULT_UART_BASE;

     enable_uart0_pin_mux();
     /* IA Motor Control Board has default console on UART3*/
     /* XXX: This is before we've probed / set board_id */
     if (board_id == IA_BOARD) {
      uart_base = UART3_BASE;
     }

     regVal = __raw_readl(uart_base + UART_SYSCFG_OFFSET);
     regVal |= UART_RESET;
     __raw_writel(regVal, (uart_base + UART_SYSCFG_OFFSET) );
     while ((__raw_readl(uart_base + UART_SYSSTS_OFFSET) &
       UART_CLK_RUNNING_MASK) != UART_CLK_RUNNING_MASK);

     /* Disable smart idle */
     regVal = __raw_readl((uart_base + UART_SYSCFG_OFFSET));
     regVal |= UART_SMART_IDLE_EN;
     __raw_writel(regVal, (uart_base + UART_SYSCFG_OFFSET));

     /* Initialize the Timer */
     init_timer();

     preloader_console_init();

     config_am335x_ddr();
     i2c1(); ----------------------------------------------------------------------------my i2c1 API
    #endif
    }

    the result still the same, the u-boot didn't execute the i2c1().

    Thanks & Regards

    Keldy

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • santosh vastrad
    Posted by santosh vastrad
    on Jul 08 2012 23:33 PM
    Expert2065 points

    HI All;

    if your paritcular i2c need to be worked means,

    which bus you are using, need to initialize in i2c_init function last line okay!

    bus_initialized[current_bus] = X; // X is the bus number

    It' will work!!!!!!!!!!

    Regards

    santosh vastrad

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use