We are planning to use AM335x chip in our new desing which will be used in medium-voltage environment. It will be a communication device mostly will interract with devices in medium voltage line devices. Because this family is quite new, i have doubt that it may fail our compatibity test. We have a big list of standarts to follow. What i want to know is with a proper desing if we use this family, do we have problems for passing test according to standarts list below or can you say this family is not intended for such industrial application?
IEC61000-6-2
IEC61000-6-4
IEC TS 61000-6-5
EN 60068-2-1 Temperature Cold Heat
EN 60068-2-2 Temperature Dry Heat
IEC 60255-5 Electrical Relays - Part 5: Insulation coordination for measuring relays and protection equipment - Requirements and tests
IEC 60255-21-1 Vibration
IEC 60255-21-2 Shock
IEC 60255-21-2 Bump
IEC 60255-21-3 Seismic
Electrical EN 50093 Voltage Dip Immunity Test
IEC 60870-2-1 Telecontrol equipment and systems - Part 2: Operating conditions - Section 1: Power supply and electromagnetic compatibility
IEC 60950-1 Dielectric
IEC 60950-1 Impulse Voltage
EMC Standards EN 61000-4-12 Oscillatory Waves Immunity Test
EN 61000-4-2 Electrostatic Discharge Immunity Test
EN 61000-4-3 Radiated Radio-Frequency Electromagnetic Field Immunity Test
Digital Radio Telephones Immunity Test
EN 61000-4-4 Electrical Fast Transient/ Burst Immunity Test
EN 61000-4-5 Surge Immunity Test
EN 61000-4-6 Immunity to conducted disturbances, induced by Radio-frequency
EN 61000-4-16 Power Frequency Test
EN 50081-2 Conducted and Radiated Emissions
EN 55024 Information Technology Equipment – Immunity
Hello,
This is a fairly long list. Is it possible to summarize the requirements from these standards so we can better answer your questions?
In general, AM335x family is being used in several industrial applications. Some of these have extended temperature requirements, some have very long lifetime requirements while few others have vibration and ESD requirements. In general, it has not been an issue so far for these applications.
Regards,
Maneesh
Dear Mr. Maneesh,
I want to use one of next list devices (AM3359ZCZD60 AM3359ZCZD72 AM3358ZCZD72 AM3357ZCZD27 AM3357ZCZD72 AM3357ZCZD60 AM3356ZCZD27 AM3356ZCZD60 AM3356ZCZD72 AM3354ZCZD60 AM3354ZCZD72 AM3352ZCZD60 AM3352ZCZD72) into industrial application which must follow next standarts
IEC61000-6-2;
IEC61000-4-2;
IEC61131-2- 92
will it be OK if i will use this chips?
Ilya