Hi,
I am using am1808 experimenters kit with NAND add on card. I would like to put kernel image and root file system along with UBL and U-BOOT. I am using SFH tool for flashing UBL and U-BOOT. can i use the same toool to flash kernel image and root file system in nand flash. If it is possible how can we do it.
Thanks
Vasu Vallabhaneni
No the, serial flasher tool is only for flashing the u-boot and UBL/SPL. and not for uImage
and filesystem. Refer this link for writing the kernel to NAND. And for filesystem, you can use
JFFS2/YAFFS just google it you should able to get it.
Thx,
--Prabhakar Lad
http://in.linkedin.com/pub/prabhakar-lad/19/92b/955