Hi,
I am trying to port ICS on SITARA. For that the kernel I am using is 3.0.1.
While booting from the kernel, it is showing the some problem with voltagedomain. Here is the log:
## Booting kernel from Legacy Image at 81000000 ...
Image Na
me: Linux-3.0.1-g000d4b0-dirty
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2769984 Bytes = 2.6 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ...
OK
Loading Kernel Image ...
Starting kernel ...
Uncompressing Linux...
done, booting the kernel.
<5>Linux version 3.0.1-g000d4b0-
dirty (dashwinee@dashwinee) (gcc version 4.4.3 (GCC) ) #3 Wed Apr 25 17:20:23 IST 2012
CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: ti8168evm
<5>Truncating RAM at 90000000-bfffffff to -afffffff (vmalloc region overlap).
<6>reserved size = 52428800 at 0
<6>FB: Reserving 52428800 bytes SDRAM for VRAM
Memory policy: ECC disabled, Data cache writeback
<7>On node 0 totalpages: 160768
<7>free_area_init_node: node 0, pgdat c0577160, node_mem_map c06cc000
<7> Normal zone: 1536 pages used for memmap
<7> Normal zone: 0 pages reserved
<7> Normal zone: 159232 pages, LIFO batch:31
<3>powerdomain: active_pwrdm: voltagedomain (null) does not exist
<3>powerdomain: default_pwrdm: voltagedomain (null) does not exist
<3>powerdomain: sgx_pwrdm: voltagedomain (null) does not exist
<3>clockdomain: alwon_mpu_clkdm: powerdomain alwon_pwrdm does not exist
<3>clockdomain: alwon_l3_fast_clkdm: powerdomain alwon_pwrdm does not exist
<3>clockdomain: alwon_ethernet_clkdm: powerdomain alwon_pwrdm does not exist
<3>clockdomain: mmu_clkdm: powerdomain alwon_pwrdm does not exist
<3>clockdomain: mmu_cfg_clkdm: powerdomain alwon_pwrdm does not exist
<3>clockdomain: active_gem_clkdm: powerdomain active_pwrdm does not exist
<3>clockdomain: sgx_clkdm: powerdomain sgx_pwrdm does not exist
<3>clockdomain: default_l3_med_clkdm: powerdomain default_pwrdm does not exist
<3>clockdomain: default_l3_slow_clkdm: powerdomain default_pwrdm does not exist
<3>clockdomain: default_ducati_clkdm: powerdomain default_pwrdm does not exist
<3>clockdomain: default_pcie_clkdm: powerdomain default_pwrdm does not exist
<7>pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768
<7>pcpu-alloc: [0] 0
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 159232
<5>Kernel command line: mem=166M@0x80000000 mem=768M@0x90000000 console=ttyO2,115200n8 androidboot.console=ttyO2 noinitrd ip=off rw init=/init root=/dev/mmcblk0p2 rootfstype=ext3 rootwait
<6>PID hash table entries: 4096 (order: 2, 16384 bytes)
<6>Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
<6>Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
<6>Memory: 166MB 462MB = 628MB total
<5>Memory: 629840k/629840k available, 64432k reserved, 0K highmem
<5>Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xffc00000 - 0xffe00000 ( 2 MB)
vmalloc : 0xf0800000 - 0xf8000000 ( 120 MB)
lowmem : 0xc0000000 - 0xf0000000 ( 768 MB)
modules : 0xbf000000 - 0xc0000000 ( 16 MB)
.init : 0xc0008000 - 0xc0037000 ( 188 kB)
.text : 0xc0037000 - 0xc0537000 (5120 kB)
.data : 0xc0538000 - 0xc0579400 ( 261 kB)
.bss : 0xc0579424 - 0xc06cb390 (1352 kB)
<6>SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
<6>NR_IRQS:376
<6>IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
<6>Total of 128 interrupts on 1 active controller
<6>GPMC revision 6.0
<4>omap_hwmod: mpu_ck: missing clockdomain for mpu_ck.
<4>omap_hwmod: gpt1_fck: missing clockdomain for gpt1_fck.
BUG: warning at arch/arm/plat-omap/dmtimer.c:354/omap_dm_timer_request_specific(): unable to get timer 1
Please somebody tell me what to do??
Thanks,
Ashwinee
Hi Anshwinee,
This forum is meant for OMAP Mobile Processor related questions. If you have questions on Sitara, please post it to:
http://e2e.ti.com/support/dsp/sitara_arm174_microprocessors/default.aspx
If you have questions on Android software please post it to:
http://e2e.ti.com/support/embedded/android/default.aspx
Regards,Satheesh
------------------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question.------------------------------------------------------------------------------------------------------------------