Hello.
I would like to clarify about the CS size which is supported on GPMC.
On TRM(spruh73g: P253), there is the description that the CS size is supported from 16Mbytes to 256Mbytes.
But, when I set GPMC_CONFIG7->MASKADDRESS = 0(CS size = 256Mbyte), I have seen the data abort.
On TRM(spruh73g: P255), there is the description that GPMC have A0-A26 address on 16bit access.
It means that max 128Mbyte address is supported.
I think GPMC CS size is max 128MByte on AM335x.
Is it correct?
Best regards,
RY