I'm trying to start up a custom board based on the AM3352ZCE and have some problems getting ethernet communications working while in u-boot.
Everything seems to be fine when looking at the signals using an oscilloscope.
I'm particularly trying to use the dhcp command to get an IP address. I have also configured a static IP address and trying to ping a machine on the LAN but it doesn't work.
Using Wireshark I see that the board sends out ARP requests and gets answers, but it doesn't seem to react on those answers. It continues to send the ARP requests.
I was wondering if anyone can give my a hint as to what I might need to fix in the u-boot configuration.
The PHY is an SMSC LAN8710.